Page top

Primary Contents

Question

Can a single Liquid Leakage Sensor Amplifiers "K7L" detect more than one liquid leakage?

Answer



Yes, it can.

It is possible to detect more than one liquid leakage with a single K7L by connecting sensing bands in parallel with use of terminal blocks

However, be aware that the sensing band where a liquid is leaked cannot be specified.

Note: 1.

When wiring, be sure not to exceed the maximum possible wiring distances for both the connecting cable and the Sensing Band. Exceeding these distances may lead to faulty operation. Connect one Sensing Band to each Terminal Block.

Note: 2.

Not applicable to K7L-AT50D

Recommended Products

E2E

Standard Sensors for Detecting Ferrous Metals under Standard Conditions

E32 Series

OMRON's Fiber Sensors continue to support an increasing range of applications.

FZ2 Series

Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.

Other Liquid Leakage Sensors FAQ