Page top

Primary Contents

Question

If D7G-F Vibration Sensor is directly mounted on a machine that sways, can it still detect earthquakes?

Answer



The D7G-F senses vibration in the X-Y direction so it cannot detect earthquakes if it is mounted directly onto the machine. Mount it on a fixed post or pillar instead.

Recommended Products

E2E

Standard Sensors for Detecting Ferrous Metals under Standard Conditions

E32 Series

OMRON's Fiber Sensors continue to support an increasing range of applications.

FZ2 Series

Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.

Other Liquid Leakage Sensors FAQ