Page top

Primary Contents

Question

How much inclination can D7E-1/-2 Vibration Sensor tolerate if it is mounted on a horizontal surface?

Answer



An inclination of 0.5° can be tolerated for horizontal mounting.

Make sure that the inclination does not exceed 0.5°.

Recommended Products

E2E

Standard Sensors for Detecting Ferrous Metals under Standard Conditions

E32 Series

OMRON's Fiber Sensors continue to support an increasing range of applications.

FZ2 Series

Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.

Other Liquid Leakage Sensors FAQ