![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Why do I get no output from the S3D2-AK[]/-CK[]/-CC[] Sensor Controller? There is one Sensor connected.
Answer
If the Sensor appears to be operating normally, that is, if the operation indicator turns ON and OFF correctly when detecting a sensing object, it is possible that the S3D2's settings are the problem.
Try setting the signal input selector for the side on which no Sensor is connected to INV (inverse). If this setting is not made, the S3D2 will not produce an output, and the OUT indicator will not turn ON.
In this condition, the indicator on the INV side will turn ON.
With the S3D2-CK[] or S3D2-CC[], the Sensor should operate by setting the AND/OR operation selector to the OR side.
Use these methods to check the Sensor.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.