Page top

Primary Contents

Question

Is it possible that sensors for Voltage Output can be connected to the Sensor Controller "S3D2"?

Answer



Sensors for Voltage Output whose NPN output can draw a current of 18mA or more can be connected to the Sensor Controller "S3D2".

Old types of Proximity Sensor "TL-G3D" or "TL-L100" (both are now discontinued) cannot be connected to the S3D2 because their NPN output can draw only about up to 2mA.

Input circuit

S3D2-AKD/-CKD/-CCD operates on 24VDC.

Recommended Products

E2E

Standard Sensors for Detecting Ferrous Metals under Standard Conditions

E3X-DA-S

An Extensive of Standard Functions to Support the World's Highest Level of Stable Detection.

FQ

Beyond simplicity. Crystal-clear imaging.

Other Sensor Controllers FAQ