Page top

Lead Contents

FAQ02312 of Emergency Stop Switches FAQ

FAQ No. FAQ02312

Primary Contents


What is diversity?


Common malfunctions and the probability of failure in electric products can be reduced if each product uses a variety of control circuits as well as various types of devices and components. The following are examples showing the use of diversity.

Safety door with safety components that use a combination of NC and NO contacts.

Circuits using control components that are different from each other in type.

Redundant combinations of electromechanical and electronic circuits.

The following diagram shows an example of operating a safety door using a combination of negative operation and positive operation switches.

Recommended Products


For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Glance.


Compact (104.5 mm), lightweight (1.3 kg) and easy-to-install Safety Laser Scanner


Supports ISO 13849-1 (PLe/Safety Category 4). Can be used on higher risk level applications by connecting to Safety Controllers.

Other Emergency Stop Switches FAQ