Page top

Lead Contents

FAQ02456 of Emergency Stop Switches FAQ

FAQ No. FAQ02456

Primary Contents

Question

Why can't a Programmable Controller or Programmable Terminal be used for the safety circuit?

Answer



The IEC 60204-1 (JIS B 9960-1) standard specifies that a safety circuit cannot be made using a programmable controller alone. This comes from the general requirement of the same standard that safety related functions must be constructed from proven circuit technology and parts. If the circuit relies on the operation of programmable electronic devices, this requirement may not be satisfied.

Recommended Products

F3SR-B

For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Glance.

OS32C

Compact (104.5 mm), lightweight (1.3 kg) and easy-to-install Safety Laser Scanner

D40Z

Supports ISO 13849-1 (PLe/Safety Category 4). Can be used on higher risk level applications by connecting to Safety Controllers.

Other Emergency Stop Switches FAQ