Page top

Lead Contents

FAQ02462 of Emergency Stop Switches FAQ

FAQ No. FAQ02462

Primary Contents


How do I replace the LED for Lighted A165E Emergency Stop Switch?


Replace the LED by separating the operation unit and the socket unit with A16Z-5080 Socket Unit lamp Extractor. Refer to the following steps 1 to 3 for the replacement procedure.

1.Removing the Socket Unit

Insert A16Z-5080 Extractor into the case guide slot shown in figure below and pull the socket unit straight out while pinching it with the Extractor.

2.Mounting the LED

The following figure shows the mounting direction. Insert the LED so that the protrusions on the LED line up with the narrow guides on the socket unit.

3.Mounting the Socket

Mount the socket unit into the operation unit. There is a specific direction for assembling the operation unit and the socket unit. Assemble the two together with the circle mark on the operation unit aligned with the L engraved in the case guide slot and press until you hear a clicking sound. Also make sure there is no lifting or other problems.

Recommended Products


For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Glance.


Compact (104.5 mm), lightweight (1.3 kg) and easy-to-install Safety Laser Scanner


Supports ISO 13849-1 (PLe/Safety Category 4). Can be used on higher risk level applications by connecting to Safety Controllers.

Other Emergency Stop Switches FAQ