Page top

Lead Contents

FAQ00760 of Digital Panel Indicators FAQ

FAQ No. FAQ00760

Primary Contents


How can a DC current of 1,000 A be measured with a K3NX Digital Panel Indicator?


Use an SDV-SH1000 Shunt, read the converted DC voltage signal at the K3NX, and scale the read value for display on the K3NX.

Note: OMRON has a wide range of Shunts available, with rated currents ranging from 5 A to 1,000 A.

The Shunt is a resistor that converts the DC current to a DC voltage.

Setting Examples:

Recommended Products


A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals


A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.


Easy to Use and Easy to Read.

Other Digital Panel Indicators FAQ