Page top

Lead Contents

FAQ01541 of Measuring / Motor Protective Relays FAQ

FAQ No. FAQ01541

Primary Contents

Question

Can the parameters of the K2CA Over Current Relay be changed during actual use?

Answer



Yes, they can because the CT (current transformer) output will not open even when the operating current or operating time parameter is changed.
However, when lowering the parameter, make sure that the current input is not lower than the operating current parameter.

Recommended Products

S8VS

Multi-Function Indication Monitor for Production Site Visualization * (* Models with indication monitor)

ZJ-FA20

High-speed, High cost performance Ionization

S8JX

Flexible Selection of Reliability and Ease of Operation with the S8JX. New Models with Harmonic Current Suppression for a Broader Lineup.

Other Measuring / Motor Protective Relays FAQ