Page top

Lead Contents

FAQ01589 of Measuring / Motor Protective Relays FAQ

FAQ No. FAQ01589

Primary Contents

Question

What precautions are necessary when the Motor Protective Relay "K2CM Series" is used in an inverter circuit?

Answer



As shown in the following figure, insert the K2CM on the secondary side of the inverter and turn OFF the reverse-phase switch before using the K2CM.

Always insert the K2CM on the secondary side (load side) of the inverter.

* Errors may occur in the operating values depending on the inverter specifications and settings. Set the values after performing tests and confirming operation.

*Use conditions differ according to wiring distance on the load side, inverter carrier frequency, basic frequency and load status. Since errors may occur in the operating values on the overload element, it is recommended to conduct an operating test before using.

Recommended Products

S8VS

Multi-Function Indication Monitor for Production Site Visualization * (* Models with indication monitor)

ZJ-FA20

High-speed, High cost performance Ionization

S8JX

Flexible Selection of Reliability and Ease of Operation with the S8JX. New Models with Harmonic Current Suppression for a Broader Lineup.

Other Measuring / Motor Protective Relays FAQ