Page top

Lead Contents

FAQ03062 of Measuring / Motor Protective Relays FAQ

FAQ No. FAQ03062

Primary Contents


What does instantaneous operation mean for Motor Protective Relays?


Instantaneous operation refers to Relays operating the instant that an overcurrent is detected. A starting current flows in motors, so Relays do not operate for a certain time during startup and then switches to instantaneous relays operation. This is referred to as instantaneous operation with a startup lock.

K2CM Motor Protective Relay Example

Overload Operating Time Characteristics for Instantaneous Type

When it is clear that a level of current exceeding the rated current will cause an error in the load, Power Supplies must be shut down immediately. Instantaneous operation is suitable for this kind of application.

Applicable models: K2CM, SE Motor Protective Relay

Recommended Products


New Models with Indication Monitor and Simple Functions for Easy System Commissioning


High-speed, High cost performance Ionization


Flexible Selection of Reliability and Ease of Operation with the S8JX. New Models with Harmonic Current Suppression for a Broader Lineup.

Other Measuring / Motor Protective Relays FAQ