Page top

Lead Contents

FAQ03139 of Measuring / Motor Protective Relays FAQ

FAQ No. FAQ03139

Primary Contents

Question

Is a specific insertion direction required, and do the input terminals have polarity for the cable of a Zero-phase Current Transformer used with an AGD/K6EL Ground Fault Relay?

Answer



No, there is no specific cable insertion direction or input terminal polarity.

Cable:

Terminal:

The cable can be inserted in either direction.

Either K or L can be connected to the input terminal of the Zero-phase Current Transformer.

*Input Terminals

AGD:

K6EL:

Z1, Z2

3, 4

Applicable models: AGD, K6EL

Recommended Products

S8VS

New Models with Indication Monitor and Simple Functions for Easy System Commissioning

ZJ-FA20

High-speed, High cost performance Ionization

S8JX

Flexible Selection of Reliability and Ease of Operation with the S8JX. New Models with Harmonic Current Suppression for a Broader Lineup.

Other Measuring / Motor Protective Relays FAQ