Page top

Lead Contents

FAQ03219 of Measuring / Motor Protective Relays FAQ

FAQ No. FAQ03219

Primary Contents

Question

What does "inverse-time operation" refer to in a Motor Relay?

Answer



This refers to a limiting motion caused by an overload factor. When a large current flows, the time until operation is shortened, and when a small current flows, the time until operation is lengthened.

The following figure shows inverse-time operation characteristics for the K2CM Motor Protective Relay.

Time Characteristics during Overload Operation
(Inverse-time Operation)

The motor itself will not burn immediately when an overcurrent is applied to it, and is generally able to withstand an overload that lasts approximately as long as the start-up time.
Inverse-time operation characteristics make it possible to prevent unnecessary operation stops by using the inrush current at start-up to trip the motor or stopping the motor when an overload condition extends for a short time.

Applicable models: K2CM, SE Motor Protective Relay

Recommended Products

S8VS

New Models with Indication Monitor and Simple Functions for Easy System Commissioning

ZJ-FA20

High-speed, High cost performance Ionization

S8JX

Flexible Selection of Reliability and Ease of Operation with the S8JX. New Models with Harmonic Current Suppression for a Broader Lineup.

Other Measuring / Motor Protective Relays FAQ