Page top

Lead Contents

FAQ04306 of Programmable Relays FAQ

FAQ No. FAQ04306

Primary Contents


ZEN Programmable Relays: How long is the cycle time for the program inside the ZEN?


The cycle time for LCD-type CPU Units is about 1 to 5 ms depending on the program structure, the number of Expansion Units connected, and RS-485 interface.

Recommended Products


A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals


A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.


Easy to Use and Easy to Read.

Other Programmable Relays FAQ