Page top

Lead Contents

FAQ04318 of Programmable Relays FAQ

FAQ No. FAQ04318

Primary Contents


ZEN Programmable Relays: How does a weekly timer function?


With a weekly timer, time ranges can be specified using days of the week and times.
They turn ON between the specified start and stop times on the specified days. If a timer is set to Tuesday through Friday: 23:00 to 05:00," then the weekly timer turns ON every day Tuesday through Friday between 23:00 and 05:00.


Recommended Products


A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals


A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.


Easy to Use and Easy to Read.

Other Programmable Relays FAQ