Page top

Primary Contents

alarm with standby sequence - Control Components Glossary

Term : alarm with standby sequence

What is 'alarm with standby sequence '? What does 'alarm with standby sequence ' mean?

Definition

An alarm equipped with a function to prevent the alarm from being output if the temperature is already in the specified alarm range when operation is started. When power is turned ON or control is started, it is first confirmed that the temperature is outside of the range in which the alarm is output. An alarm is then output if the temperature re-enters the alarm range.

Temperature Controllers