Page top

Primary Contents

output voltage variable range - In Addition Glossary

Term : output voltage variable range

What is 'output voltage variable range'? What does 'output voltage variable range' mean?

Definition

The range over which the output voltage can be varied and still maintain the specified output characteristics. Note 1: The output voltage can be adjusted beyond the output voltage variable range. The output voltage must be confirmed when adjusting it and it must be within the output voltage variable range. Note 2: The output voltage times the output current must not exceed the rated output power. The output current must not exceed the rated output current. Note 3: Do not apply excessive force to the output voltage adjuster (V.ADJ). It may break.

Power Supplies