Page top

electronic gear

Definition

The appropriate product category
A function that rotates the Servomotor for the number of pulses obtained by multiplying the command pulses by the electronic gear ratio. The electronic gear is used to synchronize the position and speed of two lines to enable using a position controller with a low command pulse frequency or to set the machine travel distance per pulse, to 0.01 mm for example.