Page top

Primary Contents

cold junction compensation

Term : cold junction compensation

What is 'cold junction compensation'? What does 'cold junction compensation' mean?

Definition

The thermo-electromotive force of the thermocouple is generated according to the temperature difference between the hot and cold junctions. If the cold junction temperature fluctuates, the measurement data will fluctuate even if the hot junction temperature remains stable. For this reason, a separate sensor built into the controller is used to monitor any changes in the cold junction (terminal connected to the thermocouple), and the controller automatically compensates for these changes to keep the cold end of the device at 0 °C. This is called cold junction compensation.

Temperature Controllers

Other Definition of cold junction compensation

Terms Applicable Categories
cold junction compensation Digital Panel Indicators