Page top

Primary Contents

remote set point input

Term : remote set point input

What is 'remote set point input'? What does 'remote set point input' mean?

Definition

For a remote set point input, the Temperature Controller uses an external input ranging from 4- to 20-mA for the target temperature. When the remote SP function is enabled, the 4- to 20-mA input becomes the set point.

Temperature Controllers