Page top

Lead Contents

Photoelectric Sensors

Photoelectric Sensors detect photo-optical workpieces. OMRON provides many varieties of Sensor, including diffuse-reflective, through-beam, retro-reflective, and distance-settable Sensors, as well as Sensors with either built-in or separate amplifiers and Fiber Units.

Primary Contents



Classification

(1) Classification by Sensing Method

1) Through-beam Sensors

Sensing Method

The Emitter and Receiver are installed opposite each other to enable the light from the Emitter to enter the Receiver. When a sensing object passing between the Emitter and Receiver interrupts the emitted light, it reduces the amount of light that enters the Receiver. This reduction in light intensity is used to detect an object.

The sensing method is identical to that of Through-beam Sensors and some models called Slot Sensors are configured with an integrated Emitter and Receiver.

Features

Stable operation and long sensing distances ranging from several centimeters to several tens of meters.

Sensing position unaffected by changes in the sensing object path.

Operation not greatly affected by sensing object gloss, color, or inclination.

2) Diffuse-reflective Sensors

Sensing Method

The Emitter and Receiver are installed in the same housing and light normally does not return to the Receiver. When light from the Emitter strikes the sensing object, the object reflects the light and it enters the Receiver where the intensity of light is increased. This increase in light intensity is used to detect the object.

Features

Sensing distance ranging from several centimeters to several meters.

Easy mounting adjustment.

The intensity of reflected light and operating stability vary with the conditions (e.g., color and smoothness) on the surface of the sensing object.

3) Retro-reflective Sensors

Sensing Method

The Emitter and Receiver are installed in the same housing and light from the Emitter is normally reflected back to the Receiver by a Reflector installed on the opposite side. When the sensing object interrupts the light, it reduces the amount of light received. This reduction in light intensity is used to detect the object.

Features

Sensing distance ranges from several centimeters to several meters.

Simple wiring and optical axis adjustment (labor saving).

Operation not greatly affected by the color or angle of sensing objects.

Light passes through the sensing object twice, making these Sensors suitable for sensing transparent objects.

Sensing objects with a mirrored finish may not be detected because the amount of light reflected back to the Receiver from such shiny surfaces makes it appear as though no sensing object is present.
This problem can be overcome using the MSR function.

4) Distance-settable Sensors

Sensing Method

The Receiver in the Sensor is either a 2-part photodiode or a position detector. The light reflected from the sensing object is concentrated on the Receiver. Sensing is based on the principle of triangulation, which states that where the beam is concentrated depends on the distance to the sensing object.

The following figure shows a detection system that uses a 2-part photodiode. The end of the photodiode nearest the case is called the N (near) end and the other end is called the F (far) end. When a sensing object reaches the preset position, the reflected light is concentrated midway between the N end and the F end and the photodiodes at both ends receive an equal amount of light. If the sensing object is closer to the Sensor, then the reflected light is concentrated at the N end. Conversely, the reflected light is concentrated at the F end when the sensing object is located farther than the preset distance. The Sensor calculates the difference between the light intensity at the N end and F end to determine the position of the sensing object.

Features of Distance-settable Sensors

Operation not greatly affected by sensing object surface conditions or color.

Operation not greatly affected by the background.

BGS (Background Suppression) and FGS (Foreground Suppression)

When using the E3Z-LS61, E3Z-LS66, E3Z-LS81, or E3Z-LS86, select the BGS or FGS function to detect objects on a conveyor belt.
The BGS function prevents any background object (i.e., the conveyor) beyond the set distance from being detected.
The FGS function prevents objects closer than the set distance or objects that reflect less than a specified amount of light to the Receiver from being detected. Objects that reflect less than a specified amount of light are as follows:

(1) Objects with extremely low reflectance and objects that are darker than black paper.

(2) Objects like mirrors that return virtually all light back to the Emitter.

(3) Uneven, glossy surfaces that reflect a lot of light but disperse the light in random directions.

Reflected light may return to the Receiver momentarily for item (3) due to sensing object movement. In that case, an OFF delay timer or some other means may need to be employed to prevent chattering.

Features

Small differences in height can be detected (BGS and FGS).

The effects of sensing object color are minimized (BGS and FGS).

The effects of background objects are minimized (BGS).

Sensing object irregularities may affect operation (BGS and FGS).

BGS_and_FGS_diagrams

5) Limited-reflective Sensors

Sensing Method

In the same way as for Diffuse-reflective Sensors, Limited-reflective Sensors receive light reflected from the sensing object to detect it. The Emitter and Receiver are installed to receive only regular-reflection light, so only objects that are a specific distance (area where light emission and reception overlap) from the Sensor can be detected. In the figure on the right, the sensing object at (A) can be detected while the object at (B) cannot.

Features

Small differences in height can be detected.

The distance from the Sensor can be limited to detect only objects in a specific area.

Operation is not greatly affected by sensing object colors.

Operation is greatly affected by the glossiness or inclination of the sensing object.

(2) Selection Points by Sensing Method

Checkpoints for Through-beam and Retro-reflective Sensors Sensing object

1. Size and shape (vertical x horizontal x height)

2. Transparency (opaque, semi-transparent, transparent)

3. Velocity V (m/s or units/min.)

Sensor

1. Sensing distance (L)

2. Restrictions on size and shape

a) Sensor

b) Retroreflector (for Retro-reflective Sensors)

3. Need for side-by-side mounting

a) No. of units

b) Mounting pitch

c) Need for staggered mounting

4. Mounting restrictions (angling, etc.)

Environment

1. Ambient temperature

2. Presence of splashing water, oil, or chemicals

3. Others

Checkpoints for Diffusion-reflective, Distance-settable, and Limited-reflective Sensors

Sensing object

1. Size and shape (vertical x horizontal x height)

2. Color

3. Material (steel, SUS, wood, paper, etc.)

4. Surface conditions (textured or glossy)

5. Velocity V (m/s or units/min.)

Sensor

1. Sensing distance (distance to the workpiece) (L)

2. Restrictions on size and shape

3. Need for side-by-side mounting

a) No. of units

b) Mounting pitch

4. Mounting restrictions (angling, etc.)

Background

1. Color

2. Material (steel, SUS, wood, paper, etc.)

3. Surface conditions (textured, glossy, etc.)

Environment

1. Ambient temperature

2. Presence of splashing water, oil, or chemicals

3. Others

(3) Classification by Configuration

Photoelectric Sensors are generally comprised of an Emitter, Receiver, Amplifier, Controller, and Power Supply. They are classified as shown below according to how the components are configured.

1) Sensors with Separate Amplifiers

Through-beam Sensors have a separate Emitter and Receiver while Reflective Sensors have an integrated Emitter and Receiver.
The Amplifier and Controller are housed in a single Amplifier Unit.

Features

Compact size because the integrated Emitter-Receiver is comprised simply of an Emitter, Receiver, and optical system.

Sensitivity can be adjusted remotely if the Emitter and Receiver are installed in a narrow space.

The signal wire from the Amplifier Unit to the Emitter and Receiver is susceptible to noise.

Typical Models (Amplifier Unit): E3C-LDA and E3C

2) Sensors with Built-in Amplifiers

Everything except the power supply is integrated in these Sensors.
(Through-beam Sensors are divided into the Emitter comprised solely of the Emitter and the Receiver comprised of the Receiver, Amplifier,and Controller.) The power supply is a tandalone unit.

Features

The Receiver, Amplifier, and Controller are integrated to eliminate the need for weak signal wiring. This makes the Sensor less susceptible to noise.

Requires less wiring than Sensors with separate Amplifiers.

Although these Sensors are generally larger than those with separate Amplifiers, those with non-adjustable sensitivity are just as small.

Typical Models: E3Z, E3T, and E3S-C

3) Sensors with Built-in Power Supplies

The Power Supply, Emitter, and Receiver are all installed in the same housing with these Sensors.

Features

Sensors can be connected directly to a commercial power supply to provide a large control output directly from the Receiver.

These Sensors are much larger than those with other configurations because the Emitter and Receiver contain additional components, such as power supply transformers.

Typical Models: E3G, E3JK, and E3JM

4) Optical Fiber Sensors

The Emitter and Receiver are connected by optical fiber.
These Sensors are comprised of a Fiber Unit and an Amplifier Unit, but the OMRON product line does not include an Amplifier Unit with a built-in power supply.

Features

Simply add a Fiber Head (end section) to make a Through-beam or Reflective Sensor.

Ideally suited to detecting very small objects.

Fiber Units are not susceptible to noise.

Typical Models (Amplifier Unit): E3X-DA-S, E3X-MDA, and E3X-NA

Recommended Products

E3Z

The New Standard for Compact, Long-range Photoelectric Sensors Conserves Energy and Natural Resources, One Million Sold Yearly

E3T

New family! Small but Sharp! Slimmest BGS(Background Suppression) Reflective Sensors in the Market.

E32 Series

OMRON's Fiber Sensors continue to support an increasing range of applications.