Page top

Lead Contents

Photoelectric Sensors

Photoelectric Sensors detect photo-optical workpieces. OMRON provides many varieties of Sensor, including diffuse-reflective, through-beam, retro-reflective, and distance-settable Sensors, as well as Sensors with either built-in or separate amplifiers and Fiber Units.

Primary Contents



Interpreting Engineering Data

Through-beam Sensors and Retro-reflective Sensors

Parallel Operating RangeExcess Gain Ratio vs. Set Distance
E3Z-T[]1(T[]6) CharacteristicsE3Z-T[]1(T[]6) Characteristics
• Through-beam Sensors: Indicates the sensing position limit for the Receiver with the Emitter at a fixed position.

• Retro-reflective Sensors: Indicates the sensing position limit for the Retroreflector when the Sensor is at a fixed position.

• Sensitivity is set to the maximum value in both cases and the area between the top and bottom lines is the detectable area.

• An area 1.5 times the area shown in the diagram is required to prevent mutual interference with more than one Through-beam Sensor installed.
• The Excess Gain Ratio shown here is the value with the sensitivity set to the maximum value.

• The rated sensing distance above is for a 15-m model. The graph shows that the Excess Gain Ratio is approximately 6 at the rated sensing distance.

Diffuse-reflective Sensors

Operating RangeSize of Sensing Object vs. Sensing Distance
E3Z-D[]1(D[]6) CharacteristicsE3Z-D[]1(D[]6) Characteristics
• Indicates the sensing start position when a standard sensing object is moved in the Y direction (vertically along the optical axis). The bottom curve in the diagram is for when the sensing object is moved from the bottom.• Indicates how the sensing distance varies with the size and surface color of the sensing object.
Note: These values are for the standard sensing object. The operating area and sensing distance will change for a different object.

Diffuse-reflective and Retro-reflective Sensors

Size of Sensing Object vs. Operating RangeObject Surface Color vs. Sensing Distance
The width and the operating range of
E3X-DA-N+E32-DC200 (example)
sensing object
The surface color and the sensing distance of
E3X-DA-N+E32-DC200 (example) sensing object
• Indicates how the operating range of the Sensor varies with the width of the sensing object.

• Each enclosed area indicates the operating area of the respective sensing object width.
• When using a Reflective Photoelectric Sensor, the surface color and gloss of the object will affect the sensing distance and the operating area.

• Indicates that the sensing distance lengthens as the reflectance of the object surface increases.
Surface Color of Object, Gloss, and Operating Range
The surface color and the operating range of E3X-DA-N+E32-DC200 (example) sensing object
• Indicates that a black object with the lowest reflectance has the smallest operating (sensing) area.

• SUS and aluminum foil are glossy and will enable a longer sensing distance. The reflection of the light by the surface, however, will only be regular reflection, not diffuse reflection, and thus the operating area will be smaller than with white paper.

Recommended Products

E3Z

The New Standard for Compact, Long-range Photoelectric Sensors Conserves Energy and Natural Resources, One Million Sold Yearly

E3T

New family! Small but Sharp! Slimmest BGS(Background Suppression) Reflective Sensors in the Market.

E32 Series

OMRON's Fiber Sensors continue to support an increasing range of applications.