Page top

Lead Contents

General Purpose Relays

OMRON provides General-purpose Relays, I/O Relays, Power Relays, Latching Relays, and Ratchet Relays.

Related Contents

Primary Contents



What Is a Relay?

Basically, a Relay is a device with contacts that opens and closes a switch as the result of an input signal (voltage or current) applied to a coil

Applications for Relays

Relays are widely used in most machines and devices that use electricity.

Types of Relays

There are mainly two types of relays: mechanical relays and solid state relays.
OMRON calls mechanical relays “General-purpose Relays.”

* For details on SSRs, refer to the Technical Explanation for Solid State Relays.

There are various types of mechanical relays (General-purpose Relays).

Hinged relays use the most common structure.

Hinged Relays

With hinged relays, the armature of the electromagnet rotates around a fulcrum. This action directly or indirectoly opens and closes a contact.

OMRON classified relays with contacts (General-purpose Relays) according to applications as shown in the following table.

TypePointsTypical Relays
Relays for control
panels
・ Control Relays
・ I/O Relays
・ Latching Relays,
etc
Relays with 1 to 4 poles are mainly
used for relay sequences or I/O
applications.
MM(K), MK(S),
MY, LY, G2R(S), G2RV,
G7T, etc.
Built-in relays
・ High -capacity
Relays, etc.
Built-in relays enable using a carry
current of up to 40 A and are used for
building into devices, e.g., to turn ON
load power supplies.
G7Z, G7J, G7X, etc.
Work-saving relays
・ Terminal Relays
・ Relay Terminals,
etc.
Work-saving relays are available in
relay units and are used mainly for I/O
applications for programmable
controllers when downsizing and
saving work are required.
G6D-F4B,
G6B-4BND, etc.
Relays for special
operations
Ratchet Relays,
etc.
Relays for special operations are
available as relays or relay units that
are specified for a specific
applications, such as alternative
operation and stepping operation of
pumps .
G4Q, G9B, MYA, etc.
Relays for PCBsThese specialized relays are mounted
on PCBs.
G5NB, G2RL, etc.

Structure and Operating Principle

General-purpose Relays transfer signals through a mechanical action.
A hinged relay is shown below as an example.
Hinged relays switch contacts by the rotating movement of an armature around a fulcrum.

Example: NO contacts (make contacts)

1. The input device (switch) is turned ON.

2. A current flows to the magnet (coil) to magnetize the core.

3. Magnetism causes the armature to be attracted to the core.
4. When the armature is attracted to the core, the moving contact touches the fixed contact and the lamp lights.
Note: At this time, the release spring is stretched out.
5. The input device (switch) is turned OFF.

6. The current to the magnetic (coil) is cut off, the force of attraction is lost, and the force of the release spring returns the armature to its original position.

7. When the armature returns to its original position, the contacts separate and the lamp turns OFF.

Application Examples:

Latching Relays (Also Called Bistable Relays or Keep Relays)
Magnetic Latching Relays: Two-coil Latching Relays

Relaxed State (after Reset)

Battery Not Connected to Coil

The diagram shows the relay in the relaxed state.
These relays are the same as the hinged relays described previously except that the core, yoke, and armature are made from semi-hard magnetic material and there are at least two coils in the relay.

Operating State (Set)

When current flows through coil A, the electromagnet (made of semi-hard material) is magnetized and the armature is attracted to the core.
As a result, the moving contact moves away from the normally closed (NC) contact (turns OFF) and makes contact with the normally open (NO) contact (turns ON).

In the set state, the residual magnetic flux in the semi-hard magnetic material (material that has properties similar to a permanent magnet) will keep the armature attracted to the core even if a current is no longer applied to coil A.

Release State (Reset) → Relaxed State

If a current is applied to coil B, which is wound in the opposite direction to coil A, the residual magnetic flux in the semi-hard magnetic material will be reduced and the magnetic attraction will weaken. The power of the release spring will become stronger than the magnetic attraction, so the armature will release and the relay will be in the relaxed state.
When the armature has released, there will be almost no residual magnetic flux in the semi-hard magnetic material.

Note:
In contrast to the hard magnetic material used in a permanent magnet, semi-hard magnetic material requires less energy to magnetize and de-magnetize.

Product Lineup

OMRON has a wide variety of General-purpose Relays so that you can select a relay that is suitable to the application.

Types of Relays (Typical Examples)

Types of Square Sockets (Typical Examples)

*Round Sockets are also available.