Page top

Primary Contents

Machine Automation Controllers

Model Ratings
NJ ---
NX ---
Note 1: The above table lists series names. Ask your OMRON representative for details on specific model numbers.
Note 2: For type approvals, these models shall not be installed on the deck, in the bridge, or on machinery that has severe vibration conditions.
Note 3: Refer to the product manuals for other application conditions.
Note 4: Noise filter TAH-06-683 manufactured by Cosel Co., Ltd. or FN-2080-XX manufactured by Schaffner or equivalent should be connected between the power terminals of NJ series and the power supply.
Type approval of the BV (Bureau Veritas) was made according to the Bureau Veritas Rules for the Classification of Steel Ships.

Programmable Controllers

Model Ratings
C200HW/C200HX/C200HG/C200HE/C200H ---
CJ1 ---
CP1 ---
CS1 ---
CV500/CV1000/CVM1/CVM1D/C500/3G2A5/3G2A9 ---
Note 1: The above table lists series names. Ask your OMRON representative for details on specific model numbers.
Note 2: For type approvals, these models shall not be installed on the deck, in the bridge, or on machinery that has severe vibration conditions.
Note 3: Refer to the product manuals for other application conditions.
Type approval of the BV (Bureau Veritas) was made according to the Bureau Veritas Rules for the Classification of Steel Ships.

Programmable Terminals

Model Ratings
NS5/NS8/NS10/NS12 ---
NA5 ---
Note 1: The above table lists series names. Ask your OMRON representative for details on specific model numbers.
Note 2: For type approvals, these models shall not be installed on the deck, in the bridge, or on machinery that has severe vibration conditions.
Note 3: Refer to the product manuals for other application conditions.
Type approval of the BV (Bureau Veritas) was made according to the Bureau Veritas Rules for the Classification of Steel Ships.