Battery-less Data Carriers with Small Memory Capacity
Note:
The 150°C heat resistance was confirmed by leaving the Unit at 150°C for 1,000 continuous hours, and by a thermal shock test consisting of 1,000 −10°C/150°C cycles of 30 min each. No defect was found among the 22 test samples.
Data Carriers with Large Memory Capacity
Note:
1. A low battery detection function is built-in.
2. The battery life is applicable for batteries used at a temperature of 25°C.The lithium battery is commercially available (CR2016).
3. The Data Carrier is dustproof when the provided battery replacement cover seal is used.
4. Data holding time: 10 years
Read/Write (R/W) Heads with Built-in Amplifier
Note:
1. Extension cables are also available. The maximum cable length is 30.5 m for the V600-H07 and 50.5 m for the V600-H11/H51/H52.
2. The connectors are not water-resistant.
Read/Write (R/W) Heads with Separate Amplifier
Note:
1. Extension cables are also available. The maximum cable length is 50 m for the V600-HA51. Extension cables are not available for the V600-HS51/HS61.
2. The connectors are not water-resistant.
ID Controllers
V600-IDSC
Transmission Distance Specifications for Battery-less Data Carriers with Small Memory Capacity
Note:
1. The transmission distance/transmission time priority mode setting can be made using the lower-level transmission mode setting switch or memory switch only with a Serial-interface Controller or ID Sensor Unit.
2. With Parallel-interface Controllers, the mode setting is always transmission distance priority.
3. The specifications take fluctuations in ambient temperature and slight differences between products into account.
Note:
1. The transmission distance/transmission time priority mode setting can be made using the lower-level transmission mode setting switch or memory switch only with a Serial-interface Controller or ID Sensor Unit.
2. With Parallel-interface Controllers, the mode setting is always transmission distance priority.
3. The specifications take fluctuations in ambient temperature and slight differences between products into account.
Note:
1. The transmission distance/transmission time priority mode setting can be made using the lower-level transmission mode setting switch or memory switch only with a Serial-interface Controller or ID Sensor Unit.
2. With Parallel-interface Controllers, the mode setting is always transmission distance priority.
3. The specifications take fluctuations in ambient temperature and slight differences between products into account.
Note:
1. The transmission distance/transmission time priority mode setting can be made using the lower-level transmission mode setting switch or memory switch only with a Serial-interface Controller or ID Sensor Unit.
2. With Parallel-interface Controllers, the mode setting is always transmission distance priority.
3. The specifications take fluctuations in ambient temperature and slight differences between products into account.
4. This is the transmission distance when using the V600-HS[]1 and V600-HA51 combination.
Note:
1. The transmission distance/transmission time priority mode setting can be made using the lower-level transmission mode setting switch or memory switch only with a Serial-interface Controller or ID Sensor Unit.
2. With Parallel-interface Controllers, the mode setting is always transmission distance priority.
3. The specifications take fluctuations in ambient temperature and slight differences between products into account.
4. This is the transmission distance when using the V600-HS[]1 and V600-HA51 combination.
Transmission Distance Specifications for Data Carriers with Large Memory Capacity (Built-in-battery/Battery-less/Replaceable-battery)
|
Note: 1. When Data Carriers are flush-mounted in metal, the read/write distance will depend on the distance (x) between the side of the DC and the metal surface.
|
2. Use the following method for flush mounting into a metallicbase.
|