ID Tags
V670_Spec1
Note: The number of accesses is the total number of read or write communications.
Antenna
V670_Spec2
Note: 1. The connector is not watertight.
2. The communications distance will be reduced if the cable is extended. The communications distance also depends on the type of extension cable used.
Controller
V670_Spec3
Note: The V670-CD1D-V1 must be used when using the V670-H51/H51Q. The V670-CD1D cannot be used.