Page top

Lead Contents

Photoelectric Sensors

Photoelectric Sensors detect photo-optical workpieces. OMRON provides many varieties of Sensor, including diffuse-reflective, through-beam, retro-reflective, and distance-settable Sensors, as well as Sensors with either built-in or separate amplifiers and Fiber Units.

Primary Contents



Explanation of Terms

ItemExplanatory diagramMeaning
Sensing
distance
Through-beam
Sensors
The maximum sensing distance that can be set with stability for Through-beam and Retro-reflective Sensors, taking into account product deviations and temperature fluctuations. Actual distances under standard conditions will be longer than the rated sensing distances for both types of Sensor.
Retro-reflective
Sensors
Diffuse-reflective
Sensors
The maximum sensing distance that can be set with stability for the Diffuse-reflective Sensors, taking into account product deviations and temperature fluctuations, using the standard sensing object (white paper). Actual distances under standard conditions will be longer than the rated sensing distance.
Limited-reflective
Sensors
As shown in the diagram at left, the optical system for the Limited-reflective Sensors is designed so that the Emitter axis and the Receiver axis intersect at the surface of the detected object at an angle θ.
With this optical system, the distance range in which regular-reflective light from the object can be detected consistently is the sensing distance. As such, the sensing distance can range from 10 to 35 mm depending on the upper and lower limits.
Mark Sensors
(Contrast scanner)
As shown in the diagram at left, the optical system for Mark Sensors is designed so that the Emitter axis is perpendicular to the detected object, and the reflected light axis intersects the Emitter axis at an angle θ. As such, the Receiver receives only diffuse reflected light, with no influence from regular reflection, and thus color detection is possible on the detected object.
Set
range/
Sensing
range
Distance-settable
Sensors
Limits can be set on the sensing position of objects with Distance-settable Sensors. The range that can be set for a standard sensing object (white paper) is called the "set range." The range with the set position limits where a sensing object can be detected is called the "sensing range." The sensing range depends on the sensing mode that is selected. The BGS mode is used when the sensing object is on the Sensor side of the set position and the FGS mode is used when the sensing object is on the far side of the set position.
Directional angle
Through-beam Sensors, Retro-reflective Sensors
The angle where operation as a Photoelectric Sensor is possible.
Differential travel
Diffuse-reflective and Distance-settable Sensors
The difference between the operating distance and the reset distance.
Generally expressed in catalogs as a percentage of the rated sensing distance.
Dead zone
The Dead zone outside of the emission and reception areas near the lens surface in Mark Sensors, Distance-settable Sensors, Limited reflective Sensors, Diffuse-reflective Sensors, and Retro-reflective Sensors.
Detection is not possible in this area.
Response time
The delay time from when the light input turns ON or OFF until the control output operates or resets. In general for Photoelectric Sensors, the operating time (Ton) ≈ reset time (Toff).
ItemExplanatory diagramMeaning
Dark-ON
operation
(DARK ON)
The "Dark-ON" operating mode is when a Through-beam Sensor produces an output when the light entering the Receiver is interrupted or decreases.

The "Light-ON" operating mode is when a Diffuse-reflective Sensor produces an output when the light entering the Receiver increases.
Light-on
operation
(LIGHT ON)
Ambient
operating
illumination
The ambient operating illumination is expressed in terms of the Receiver surface illuminance and is defined as the illuminance when there is a ±20% change with respect to the value at a light reception output of 200 lx. This is not sufficient to cause malfunction at the operating illuminance limit.
Standard
sensing
object
The standard sensing object for both Through-beam Sensors and Retro-reflective Sensors is an opaque rod with a diameter larger than the length of a diagonal line of the optical system.
In general, the diameter of the standard sensing object is the length of the diagonal line of the Emitter/Receiver lens for Through-beam Sensors, and the length of a diagonal line of the Reflector for Retro-reflective Sensors.

Size of standard sensing object Using Reflector
Reflector modelsDiagonal line of
optical system
Sensing
object
E39-R1/R1S/R1K72.2 mm75-mm dia.
E39-R2100.58 mm105-mm dia.
E39-R341.44 mm45-mm dia.
E39-R426.77 mm30-mm dia.
E39-R656.57 mm60-mm dia.
E39-R943.7 mm45-mm dia.
E39-R1066.47 mm70-mm dia.
E39-RS136.4 mm40-mm dia.
E39-RS253.15 mm55-mm dia.
E39-RS3106.3 mm110-mm dia.
E39-R3713.4 mm15-mm dia.
For Diffuse-reflective Sensors, the standard sensing object is a sheet of white paper larger than the diameter of the emitted beam.
Minimum
sensing
object
Typical examples are given of the smallest object that can be detected using Through-beam and Retro-reflective Sensors with the sensitivity correctly adjusted to the light-ON operation level at the rated sensing distance.

For Diffuse-reflective Sensors, typical examples are given of the smallest objects that can be detected with the sensitivity set to the highest level.
Minimum
sensing
object
with slit
attached
Through-beam Sensors
Typical examples are given of the smallest object that can be detected using Through-beam Sensors with a Slit attached to both the Emitter and the Receiver as shown in the figure. The sensitivity is correctly adjusted to the Light-ON operating level at the rated sensing distance and the sensing object is moved along the length and parallel to the slit.

Application and Data

(1)Relationship of Lens Diameter and Sensitivity to the Smallest Detectable Object

With a Through-beam Sensor, the lens diameter determines the size of the smallest object that can be detected.

With a Through-beam Sensor, a small object can be more easily detected midway between the Emitter and the Receiver that it can be off center between the Emitter and Receiver.

As a rule of thumb, an object 30% to 80% of the lens diameter can be detected by varying the sensitivity level.

Check the Ratings and Specifications of the Sensor for details.

The size given for the smallest object that can be detected with a Reflective Photoelectric Sensor is the value for detection with no objects in the background and the sensitivity set to the maximum value.

Maximum sensitivityAdjusted sensitivity
Detects objects 80% of the lens diameter.Detects objects up to 30% of the lens diameter.

(2) Detecting Height Differences

Selecting Sensors Based on Detectable Height Differences and Set Distances (Typical Examples)

Selecting_Sensors_Based_on_Detectable_Height_Differences_and_Set_Distances_diagrams

(3) MSR (Mirror Surface Rejection) Function

Principles

This function and structure uses the characteristics of the Retroreflector and the polarizing filters built into the Retro-reflective Sensors to receive only the light reflected from the Retroreflector.

The waveform of the light transmitted through a polarizing filter in the Emitter changes to polarization in a horizontal orientation.

The orientation of the light reflected from the triangular pyramids of the Retroreflector changes from horizontal to vertical.

This reflected light passes through a polarizing filter in the Receiver to arrive at the Receiver.

Purpose

This method enables stable detection of objects with a mirror-like surface.
Light reflected from these types of objects cannot pass through the polarizing filter on the Receiver because the orientation of polarization is kept horizontal.

Examples

A sensing object with a rough, matte surface (example (2)) can be detected even without the MSR function. If the sensing object has a smooth, glossy surface on the other hand (example (3)), it cannot be detected with any kind of consistency without the MSR function.

(1) No Object(2) Non-glossy Object(3) Object with a Smooth, Glossy Surface(Example: battery, can, etc.)
The light from the Emitter hits the Reflector and returns to the Receiver.Light from the Emitter is intercepted by the object, does not reach the Reflector, and thus does not return to the Receiver.Light from the Emitter is reflected by the objectand returns to the Receiver.

Caution

Stable operation is often impossible when detecting objects with high gloss or objects covered with glossy film. If this occurs, install the Sensor so that it is at an angle off perpendicular to the sensing object.

Retro-reflective Sensors with MSR function

Retro-reflective Sensors with MSR function
Classification by ConfigurationModel
Optical Fiber SensorsE32-R21, E32-R16
Built-in Amplifier SensorsE3Z-R61/R66/R81/R86
E3ZM-R61/R66/R81/R86/B61/B66/B81/B86
E3ZM-CR61(-M1TJ)/CR81(-M1TJ)
E3S-CR11(-M1J)/CR61(-M1J)
E3S-CR62/67
Separate Amplifier SensorsE3C-LR11/LR12
Built-in Power Supply SensorsE3JM-R4[]4(T), E3JK-R2M[]/R2S3
Transparent Object SensorsE3S-R11/R31/R61/R81/R16/R36/R66/R86

Note:When using a Sensor with the MSR function, be sure to use an OMRON Reflector

Retro-reflective Sensors without MSR Function

When detecting a glossy object using a Retro-reflective Sensor without the MSR function, mount the Sensor diagonally to the object so that reflection is not received directly from the front surface.

Retro-reflective Sensors without MSR Function
Classification by ConfigurationModel
Transparent Object SensorsE3Z-B61/B62/B66/B67/B81/B82/B86/B87
E3S-R12/R62/R17/R67

Selecting Transparent Object Sensors

Use the following procedure to select an appropriate Transparent Object Sensor.

Selecting_Transparent_Object_Sensors_diagram

(4) Surface Color and Light Source Reflectance

Surface Color Reflectance

Reflectance of Various Colors at Different Wavelengths of Light

Identifiable Color Marks

Applicable Sensor Light Colors: : Red light source : Green light source : Blue light source
Sensors with a RGB light source can detect all combinations.

These figures represent typical examples of ratios for light reflected by the back and mark.

Sensor light colorProduct classificationModel
Red light source
Optical Fiber SensorsE3X-DA-S
E3X-NA
Separate Amplifier SensorsE3C-VS3R
E3C-VM35R
E3C-VS7R
Blue light source
Optical Fiber SensorsE3X-DAB-S
Green light source
Optical Fiber SensorsE3X-DAG-S
E3X-NAG
Separate Amplifier SensorsE3C-VS1G
RGB light source
(or white light)
Built-in Amplifier SensorsE3MC-A
Optical Fiber SensorsE3MC-X/Y
E3X-DAC-S

(5) Self-diagnosis Functions

The self-diagnosis function checks for margin with respect to environmental changes after installation, especially temperature, and informs the operator of the result through indicators and outputs. This function is an effective means of early detection of product failure, optical axis displacement, and accumulation of dirt on the lens over time.

Principles

These functions alert the operator when the Sensor changes from a stable state to an unstable state. The functions can be broadly classified into display functions and output functions.

Display function

Stability Indicator (green LED)
The amount of margin with respect to environmental changes (temperature, voltage, dust, etc.) after installation is monitored by the self-diagnosis function and indicated by an indicator. (Illuminates steadily when there are no problems.)

Operation Indicator (Orange LED)
Indicates the output status.

Output function

The margin is indicated by an indicator light, and the state is output to alert the operator.

Purpose

Self-diagnosis functions are effective in maintaining stable operation, alerting the operator to displacement of the optical axis, dirt on the lens (Sensor surface), the influence from the floor and background, external noise, and other potential failures of the Sensor.

Display_and_Output_function_diagrams

Example: Light-ON Operation

Indicator stateLight-ON/Dark-ON indicated bythe orange indicatorDegree of margin with respect to temperature changes indicated by the green indicatorSelf-diagnosisoutputExample of diagnosed condition
Light Incident
(orange indicator ON)
Stable use is possible.
(Margin of 10% to 20% or higher)
(Stability indicator: ON)
The margin is not
sufficient.
(Green indicator: OFF)
When this state
continues for a
certain period
of time, an
output alerts
the operator.
Light
Interrupted
(orange indicator OFF)
Stable use is possible.
(Margin of 10% to 20% or higher)
(Stability indicator: ON)

Applicable Models

Classification by ConfigurationModelsSelf-diagnosis function
Display functionOutput function
Optical Fiber SensorsE3X-DA-SDigital display
E3X-MDADigital display---
E3X-NA
Separate Amplifier SensorsE3C-LDADigital display
E3C●(E3C-JC4P)
Built-in Amplifier SensorsE3Z*
E3ZM(-C)---
E3T---
E3S-C---
E3S-CL---
E3S-CR62/67---
E3S-R---

* Contact your OMRON representative regarding E3Z models with self-diagnosis output.

(6) External diagnosis input function (emission stop function)

Principle

The pink to blue wires in the Through-beam Emitter cable can be short-circuited to stop light emission at any timing. When there is no object between the Emitter and the Receiver, turning the light Emitter ON and OFF should cause the Receiver output to turn ON and OFF. Otherwise, there is a problem.

Purpose

This function allows the operator to check the operation of the Sensor before work begins.

Example: E3Z-T62-G0 Emitter

Example: DARK ON Mode

Key Points

If the control output changes when the external diagnosis input is turned ON and OFF, the Sensor is normal. If the control output remains ON or remains OFF, the Sensor is faulty.

Note:When using the external diagnosis input function, it is assumed that the object does not interrupt the Sensor being checked from light.

E3Z-T62G0

External diagnosis
input OFF
(blue-pink open)
Light emissionControl output OFF

External diagnosis check

External diagnosis
input ON
(blue-pink shorted)
Light emission stops
(electrically creates a DARK
ON state due to object)
Control output ONNormal
Control output OFFAbnormal

Recommended Products

E3Z

The New Standard for Compact, Long-range Photoelectric Sensors Conserves Energy and Natural Resources, One Million Sold Yearly

E3T

New family! Small but Sharp! Slimmest BGS(Background Suppression) Reflective Sensors in the Market.

E32 Series

OMRON's Fiber Sensors continue to support an increasing range of applications.