Page top

Three case studies of worldwide Use of NX1

The NX1 Machine Automation Controller that controls devices at manufacturing sites is also used in infrastructures and facilities. This page provides three case studies.

Why the NX1 Controller is highly appreciated in manufacturing and other sectors

Information utilization

  • Direct access to databases without the need for PCs ensures reliable data transfer.
  • Connectivity to OPC UA and other leading-edge networks helps maintain network reliability and security and access cloud services.
  • Advanced control in miniaturized size

  • CPU, power supply, and Ethernet ports are housed in a compact design with a width of 66 mm.

Omron’s extensive product portfolio and total support

  • The NX1 for industrial use is more robust than PCs.
  • International standard IEC 61131-3 (PLCopen) programming is supported.
  • The diverse lineup of over 200,000 products includes inputs, outputs, and safety.
Why the NX1 Controller is highly appreciated in manufacturing and other sectors

Case 1:
Parking and refueling management system at airport

Case 1: Parking and refueling management system at airport

A Malaysian airport company decided on the NX1 as the controller for its billing system.
This system monitors the amount of time an aircraft is parked on the apron and the amount of supplied fuel and transfers the data directly to the database.
The airport company charges airlines for parking and refueling based on this data.

The NX1 was chosen for its robustness and various IoT connectivity options (SQL, OPC UA). Another appreciated benefit was Omron’s high-quality technical support.

Case 1: Configuration of parking and refueling management system at airport

Case 2:
Waste compactor at shopping mall

Case 2: Waste compactor at shopping mall

The NX1 is also used for a new type of waste compactor.
Waste from the shopping mall or sport facility is compressed in the compactor installed on the site. The compacter helps manage when to collect the compressed waste for disposal and calculate how much to bill.

The compact NX1 Controller integrated into the compactor can transmit the waste amount and other data directly to the database while controlling the motors and safety components. This eliminates the need for PCs, improving redundancy and reliability.

Since all machine data will be collected in the cloud in the future, the NX1 that supports secure OPC UA was selected.

Case 2: Configuration of waste compactor at shopping mall

Case 3:
Propane vending machine

Case 3: Propane vending machine

The NX1 has been employed to control propane vending machines in Norway.

Customers just put their own gas cylinders in the machine and operate the touchscreen to fill the cylinders with the desired amount of gas.

The NX1 controls all devices in the vending machine without human intervention 24 hours a day, saving labor costs.
Omron can offer not only space-saving compact controllers but also sensors, inverters, and all other devices required for the machine. Its excellent technical support was also one of the key factors determining use of the NX1.

Case 3: Configuration of propane vending machine


Photographs are for illustration purposes only and do not represent actual applications.
Images used under license from Shutterstock.com.
The system configurations in this page are for reference purposes only.
Sysmac is a trademark or registered trademark of OMRON Corporation in Japan and other countries for OMRON factory automation products.
EtherCAT® is a registered trademark and patented technology, licensed by Beckhoff Automation GmbH, Germany.
Safety over EtherCAT® is a registered trademark and patented technology, licensed by Beckhoff Automation GmbH, Germany.
EtherNet/IP™, CIP Safety™, CompoNet™, and DeviceNet™ are trademarks of ODVA.
OPC and OPC UA are trademarks of the OPC Foundation.
Other company names and product names in this page are the trademarks or registered trademarks of their respective companies.
Microsoft product screen shot(s) reprinted with permission from Microsoft Corporation.
The product photographs and figures that are used in this page may vary somewhat from the actual products.