Page top

Information in your hand  Take the next step of on-site IoT

NX1
Retrofittable - Advanced functionality in miniaturized size -
Real-time - Collection of useful production data -
Seamless - Integration of control and information -

Retrofittable

IoT for existing production lines

2 EtherNet/IP ports and 1 EtherCAT port

3 built-in industrial Ethernet ports

  • EtherNet/IP
  • EtherCAT

Connect to existing networks via
2 EtherNet/IP ports and 1 EtherCAT port.

Supports various networks

OPC UA and SLMP certified NX1 ensures
secure connections to existing networks.

Supports various networks
OPC UA What is OPC UA?

OPC Unified Architecture (OPC UA), also known as IEC 62541, is an open industrial communication protocol that enables secure and reliable data exchange between products from different vendors and across operating systems.
OPC UA is listed as a recommendation for the communication technology in Reference Architecture Model Industrie 4.0 (RAMI 4.0), which has attracted interest worldwide.
In addition, this standard is integrated with the IEC 61131-3 PLC programming standard to reliably exchange field data from machines to IT systems like MES or ERP, serving as a basis for the packaging standard PackML (ANSI/ISA-TR88) and the standard for exchange of data between injection molding machines (EUROMAP 77).
Since the adoption of this open standard is increasing across the world, we are implementing OPC UA functionality as a standard feature of our NX102/NJ501 Machine Automation Controller. We are contributing to the diffusion of the industrial IoT standard, providing a bridge between industrial automation and information technology.

Slim design only 66 mm wide

CPU, power supply,
and Ethernet ports
in slim housing!

Real-time

  • Collection of useful production data

    Useful data can be collected in synchronization with the production cycle and control cycle.
  • Real-time traceability

    Real-time full traceability

    The NX1 can verify 1,000 products per minute (approximately 60 ms per product), enabling traceability of all products without increasing the production cycle time.

  • Fast data collection for predictive maintenance

    Synchronized data can be stored in a database within the same fixed cycle time of 1 ms, allowing you to understand machine behavior more accurately.

Seamless

Integration of control and information

Integration of control and information

Based on our long experience,
we bring IoT to production sites using the controller that integrates control and information.
A key element is the use of a multicore processor.

Multicore processor

Multicore processor

The NX1 maximizes the multicore processor’s performance to control a machine and utilize data at the same time without compromising control performance.
This enables a single controller to provide
full product traceability during motion control.

Application case study

Food manufacturer
Improve accuracy of liquid filling quantity and collect filling quantity data

Improve accuracy of liquid filling quantity and collect filling quantity data
Problem The quantity of liquid food filled in bottles is inconsistent. If the filling quantity is more than the specified quantity, it can lead to company’s loss. If less than the specified quantity, it can lead to complaints from consumers.
Request To manage production records, filling quantities need to be written into a database without affecting control of the filling process. Monitoring uptime across the production line will be required in the future.
Benefit
The NX1 Controller combined with the NX-RS Load Cell Input Unit can write the filling quantity to the database using database direct connection functionality while controlling filling at high speeds with high precision. This enables production log management. Its OPC UA functionality can be used for information utilization for the entire production line in the future.


Sysmac is a trademark or registered trademark of OMRON Corporation in Japan and other countries for OMRON factory automation products.
EtherCAT® is a registered trademark and patented technology, licensed by Beckhoff Automation GmbH, Germany.
Safety over EtherCAT® is a registered trademark and patented technology, licensed by Beckhoff Automation GmbH, Germany.
EtherNet/IP™, CIP Safety™, CompoNet™, and DeviceNet™ are trademarks of ODVA.
OPC and OPC UA are trademarks of the OPC Foundation.
Other company names and product names in this page are the trademarks or registered trademarks of their respective companies.
Microsoft product screen shot(s) reprinted with permission from Microsoft Corporation.
The product photographs and figures that are used in this page may vary somewhat from the actual products.