faq00454- ...s Primary Contents Question What system configuration is necessary to display the contents of 4-digit decimal data memory in Programmable Controllers on an external 7-segment digital display?...
https://www.ia.omron.com/support/faq/answer/26/faq00454/
faq00923- ...AQ No. FAQ00923 Related Contents Primary Contents Question How do I create a program to input 2-digit BCD data from a digital switch to CIO 0.08 to CIO 0.15 and then move the data to specifie...
https://www.ia.omron.com/support/faq/answer/26/faq00923/
faq00924- ... No. FAQ00924 Related Contents Primary Contents Question How do I create a program to input 1.5-digit BCD data to CIO 0.00 to 0.05 BCD from a digital switch and move it to a specified DM Area...
https://www.ia.omron.com/support/faq/answer/26/faq00924/
faq00925- .... FAQ00925 Related Contents Primary Contents Question How do I make a program to transfer a 2.5-digit BCD data stored in the DM Area to display it on a static-input digital display (CIO 2.00 ...
https://www.ia.omron.com/support/faq/answer/26/faq00925/
faq01076- ...tch is input to CIO 0 bits 00 to 09 and moved to D102. The numbers stored in D102 are shifted 1 digit (4 bits) to the right whenever numbers are input using the ten-key. If 5 or more digits a...
https://www.ia.omron.com/support/faq/answer/26/faq01076/
faq01077- ... is summarized here. Figure3 Calculation A: Use the ADD WITHOUT CARRY instruction for rightmost digit calculations in which there is no carry from the lower digit. Calculation B: Use...
https://www.ia.omron.com/support/faq/answer/26/faq01077/
faq01107- ...ke the C200HX/HG/HE-Z compatible with the C200HX/HG/HE, expansion instructions can be set, or 3-digit function codes can be used. Also, symbol instructions can also be used. 3.Extended Data M...
https://www.ia.omron.com/support/faq/answer/26/faq01107/
faq02069- ...xample 1: Relatively Simple Calculation Use BINARY ADD An internal offset value is added to a 4-digit BCD input value from a thumbwheel switch, and the result is output as a 4-digit ...
https://www.ia.omron.com/support/faq/answer/26/faq02069/
faq02260- ...s. *When one of the pushbutton switches from 1 to 32 is pressed, the two words of input data (4-digit BCD data) will be stored in D100 to D131 as shown in the following example. Programming: ...
https://www.ia.omron.com/support/faq/answer/26/faq02260/
faq02492- ...o indicate a negative number. Additional Information What Is a Tan's Complement? a.Subtract a 4-digit BCD value from 9,999 or an 8-digit BCD value from 99,999,999. The ten's compleme...
https://www.ia.omron.com/support/faq/answer/26/faq02492/