faq02060- ...changeable. Note:These Relays are socket-mounted plug-in type. The Sockets are separately sold. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/36/faq02060/
faq02062- ...N Relays model number. Specify the coil voltage after the model number as shown in the example. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/36/faq02062/
FAQ02098 for General Purpose Relays | OMRON Indust...- ...table depending on an applied load. Surge protection suitable for the applied load is required. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/36/faq02098/
faq02104- ...DC Maximum switching current 5 A Contact form DPDT Contact structure Single Contact material Ag MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/36/faq02104/
FAQ02139 for General Purpose Relays | OMRON Indust...- ...s, refer to the following table. Be careful not to apply other voltages than the rated voltage. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/36/faq02139/
FAQ02147 for General Purpose Relays | OMRON Indust...- ...0 -6 /operation means that 1/10,000,000 failures can be expected at a reliability level of 60%. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/36/faq02147/
FAQ02165 for General Purpose Relays | OMRON Indust...- ...0 Relay Approx. 2 to 3 Capacitor Approx. 20 to 50 Resistive load 1 DC Loads and Inrush Current: MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/36/faq02165/
faq02190- ... the NO contacts close before the NC contacts open. These are also called "continuous contacs." MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/36/faq02190/
faq02198- ...pose Relays Socket. It cannot be connected to PCB terminals, such those on G2R-1 or G2R-2A PCB. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/36/faq02198/
FAQ02207 for General Purpose Relays | OMRON Indust...- ...et voltage I: Load (relays etc.) reset current I L : Leakage current from the Solid-state Relay MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/36/faq02207/