...he ratio of the incident light to the threshold, expressed as follows: Incident light/Threshold x 100 (%). The margin shows whether the operation of the sensor is stable. This term is formall...
...he ratio of the incident light to the threshold, expressed as follows: Incident light/Threshold x 100 (%). The margin shows whether the operation of the sensor is stable. It is also simply ca...
...vo Drivers The power rate is given by this formula: Power rate = (Rated torque) 2/Rotor inertia x 10-3. The higher the value is, the better the response is. The unit is (kW/s)....
...and it is the amount of work done by electricity in one second. Power (watts) = Voltage (volts) x Current (amperes) W = V x I The unit is the watt (W). Power consumption is the amoun...
...ject Ferrous metal (Sensitivity lowers with non-ferrous metals.) Standard sensing object Iron 5 x 5 x 1 mm Response frequency 1 kHz (Average value) Power supply voltage 5 to 24 VDC r...