Classifications of Solid-state Relays | OMRON Indu...- ...o- coupler G3H G3B G3F G3NA (AC input) No Phototriac G3NE G3J G3F G3H G3TA-OA Yes *1 Phototriac G3PA-VD G3PE (single phase) G3NA (DC input) G3NE Yes *1 Phototriac G3PE-2(N) (three phases) *2 ...
https://www.ia.omron.com/support/guide/31/classifications.html
Relays - CE Marking - Europe, Pan European | OMRON...- ...del/Combination EMC Directive Low-voltage Directive Machinery Directive G32A ● ● Not Applicable G3PA-2[]-VD G3PA-4[]-VD G3NA-UTU G3NE-US G3H-VD G3F-VD G3HD-VD G3FD-VD G3PE G3PF G3PC-...
https://www.ia.omron.com/support/models/en/relay.html
Relays - UKCA Marking (Machinery, Low-Voltage, EMC...- ...pment (Safety) Reg. Supply of Machinery (Safety) Reg. Safety Category G32A ● ● Not Applicable 1 G3PA-2[]-VD G3PA-4[]-VD G3NA-UTU G3NE-US G3H-VD G3F-VD G3HD-VD G3FD-VD G3PE G3PF G3PH ...
https://www.ia.omron.com/support/models/ukcames/relay.html
Relays - VDE Certification - Europe, Germany | OMR...- ...FOM16 --- EN 50178 125362 Top of page Solid-state Relays Model Ratings Standard No. License No. G3PA-210B-VD 10A 240V AC EN62314 5915 G3PA-220B-VD 20A 240V AC EN62314 5915 ...
https://www.ia.omron.com/support/models/vde/relay.html
faq02044- ...or Solid-state Relays with DC inputs that use a constant current input method (such as G3NA and G3PA). Ratings Applicable model Item Rated voltage Operating voltage Impedance Model ○ G3H-203S...
https://www.ia.omron.com/support/faq/answer/18/faq02044/
FAQ02075 for Solid-state Relays | OMRON Industrial...- ...he output elements. 2.The following models have a built-in surge-absorbing varistor: G3NA, G3S, G3PA, G3PB, G3NE, G3J, G3NH, G9H, G3DZ (some models), G3RZ, G3FM 3.Be sure to take measures aga...
https://www.ia.omron.com/support/faq/answer/18/faq02075/
faq03640- ...e Relays. Example: Load Current Vs. Ambient Temperature Rating for High-density or Gang-mounted G3PA-220B-VD Solid-state Relays. For G3PA the following conditions apply when using hi...
https://www.ia.omron.com/support/faq/answer/18/faq03640/
Further Information of Temperature Controllers | O...- ...table SSRs *1. Two G3PE-BL SSRs can be connected. *2. One G3PE-BL SSR can be connected. *3. Two G3PA-BL SSRs can be connected. *4. One G3PA-BL SSR can be connected. *5. Two of the -U...
https://www.ia.omron.com/support/guide/53/further_information.html
Relays - UL Certification - Americas, US and Canad...- ...on of UL Standard Model Ratings Standard No. File No. Category Listed/Recognized Output Ratings G3PA-210B-VD --- UL508 E64562 NMFT2, NMFT8 Recognized 10A 240V AC G3PA-220B-VD --- UL5...
https://www.ia.omron.com/support/models/ul/relay.html
Safety Precautions of Solid-state Relays Cautions ...- ...sistance, use the following formula. For SSRs with constant-current input circuits (e.g., G3NA, G3PA, G3PE, G3PJ), calculation is performed at 0.1 mA. 3. ON/OFF Frequency An SSR has delay tim...
https://www.ia.omron.com/product/cautions/18/safety_precautions.html