...ve the rubber cap and check that the set bolt is loose. 2. Insert the Servomotor shaft into the input shaft. 3. Tighten the Servomotor installation bolt according to the tightening torque spe...
...ys Lead Contents FAQ No. FAQ02279 Related Contents Primary Contents Question What is an inverse input? Answer An inverse input is an input that creates a potential differe...
...en there is no reset switch in the feedback circuit and the device automatically starts when an input turns ON. A manual reset is when there is a reset switch in the feedback circuit and the ...
... Contents FAQ No. FAQ02416 Related Contents Primary Contents Question What is a positive common input? Answer It is an input mode where there are two inputs and both of them are co...
...nt. Solid-state Relays with a zero cross function using a photocoupler can operate with a small input current because they have very good coupler transmission efficiency. Photocoupler ...
...state Relays Lead Contents FAQ No. FAQ02044 Related Contents Primary Contents Question Does the input current change for Solid-state Relays with a wide rated input voltage? Answer ...
...ng Method Connect a load and power supply, and check the voltage of the load terminals with the input ON and OFF. The output voltage will be close to the load power supply voltage with the SS...
... those of the G2R-1A-S and so these models can be easily exchanged. Note:Be sure to confirm the input voltage, polarity, and output capacity. 3.Applications with high-voltage DC loads. To swi...
...tate Relay load Relays sometimes hum? Answer Leakage current flows when the Solid-state Relay input is OFF. If a small Relay is driven, this Leakage current may cause the Relay coil to beco...
...r AC load switching use thyristors and triacs as output elements. By turning Solid-state Relays input ON, the output can be turned ON, but simply turning the input OFF doesn't mean t...