...tored water Definition The appropriate product category Level Switches Water that is stored for a purpose. Most of the time its sensitivity is same as tap water. The use of water as fire-figh...
...tomation limit cycle method Definition The appropriate product category Temperature Controllers A method used to calculate the PID constants according to the hunting cycle and oscillations ob...
...strial Automation remote SP Definition The appropriate product category Temperature Controllers A set point that is input with an external analog signal....
... remote set point input Definition The appropriate product category Temperature Controllers For a remote set point input, the Temperature Controller uses an external input ranging from 4- to ...
...l Automation remote control function Definition The appropriate product category Power Supplies A function that allows the output voltage of the Power Supply to be turned ON and OFF from an e...
...on The appropriate product category Power Supplies Remote sensing can be used to compensate for a voltage drop on the load lines. (The compensation range is ±10% of the rated output voltage.)...
...ory Programmable Controllers Programming and monitoring PLCs and other devices on networks from a direct cable connection to a PLC or other network device....
...omation cooling coefficient Definition The appropriate product category Temperature Controllers A cooling coefficient is used when the heating characteristics and cooling characteristics of t...
...tion The appropriate product category Limit Switches The force required to move the actuator of a Fork Lever Lock Switch from the free position to the reverse operation position....