...utomation set point limiter Definition The appropriate product category Temperature Controllers A limit within which the set point range is controlled to prevent a controlled object ...
...n control output assignment Definition The appropriate product category Temperature Controllers A function for assigning the manipulated variable, transfer output, alarm output, or other func...
...omation valve-control model Definition The appropriate product category Temperature Controllers A Temperature Controller that can perform position-proportional control. The Temperature Contro...
...al Automation robust tuning Definition The appropriate product category Temperature Controllers A method for automatically setting the PID constants according to characteristic changes in the...
...l Automation thyristor unit Definition The appropriate product category Temperature Controllers A switching element used to control power. There are SCR (product name: Three-pole Conductive T...
...product category Temperature Controllers The characteristics of the controlled object including a time element. The dynamic characteristics describe the relationship between the inputs and ou...
...mation external disturbance Definition The appropriate product category Temperature Controllers A quantity that disturbs the status of the control system....
...ation sheathed thermocouple Definition The appropriate product category Temperature Controllers A thermocouple in which the protective tube and thermocouple elements are insulated with magnes...
...mation manipulated variable Definition The appropriate product category Temperature Controllers A variable used to change the control amount for the controlled object to make it agree with th...
...opriate product category Temperature Controllers Operation in which the output value changes in a reverse proportion to the process value, i.e., the output value becomes smaller as the proces...