...ustrial Automation rated voltage Definition The appropriate product category Solid-state Relays A voltage that serves as a standard for the input signal....
...te product category Solid-state Relays The current that can flow into the output terminals when a specified load voltage is applied to the SSR with the output turned OFF....
...product category Level Switches The instantaneous current that flows when the contacts close or a transitive current that is higher than the steady-state current....
...dustrial Automation SP ramp Definition The appropriate product category Temperature Controllers A function that prevents step-wise changes in the set point by increasing or decreasing the set...
...trial Automation MB command Definition The appropriate product category Temperature Controllers A SYSWAY (Host Link) command. This command is used to enable and disable writing with communica...
...nd Definition The appropriate product category Temperature Controllers The width used to detect a loop burnout alarm. If the process value does not change by this value even though the manipu...
...ion MB Command Logic Switch Definition The appropriate product category Temperature Controllers A parameter used to set the logic used by the SYSWAY MB command to enable/disable writing via c...
...ernal power supply for ES1B Definition The appropriate product category Temperature Controllers A 12-VDC power supply for an ES1B Infrared Temperature Sensor....
...ppropriate product category Programmable Terminals An acronym for super-twisted nematic. STN is a type of liquid crystal display. The disadvantages of STN LCDs are slow response and poor imag...
...brightness Definition The appropriate product category Programmable Terminals The brightness of a display device measured in cd (candela). A higher candela value means a bri...