FAQ01267 for Ultrasonic Sensors | OMRON Industrial...- ... temperature that the Ultrasonic Sensor can be used in? Answer 55 °C, but the power supply of E4R Ultrasonic Sensor Amplifier should not be used in an ambient temperature higher than 40 °C....
https://www.ia.omron.com/support/faq/answer/50/faq01267/
FAQ01272 for Ultrasonic Sensors | OMRON Industrial...- ...negligible. Refer to the parallel movement characteristics diagram when spacing the Sensors. 3. E4R Ultrasonic Sensor Standard Pulse Unit When using multiple E4R-2 Power Supplies at ...
https://www.ia.omron.com/support/faq/answer/50/faq01272/
FAQ01284 for Ultrasonic Sensors | OMRON Industrial...- ...swer The following Sensors can be used. E4A-3K Ultrasonic Sensor E4C Series Ultrasonic Sensor E4R Series Ultrasonic Sensor E2E Standard Sensors for Detecting Ferrous Metals under Standard C...
https://www.ia.omron.com/support/faq/answer/50/faq01284/
FAQ01281 for Ultrasonic Sensors | OMRON Industrial...- ...r than 100 m. Use a cable with conductor cross section of at least 0.3 mm 2 . 4. E4C Series and E4R Series The cable between the Sensor and the Amplifier Unit (labeled as 1 below) must not be...
https://www.ia.omron.com/support/faq/answer/50/faq01281/
faq01281- ...r than 100 m. Use a cable with conductor cross section of at least 0.3 mm 2 . 4. E4C Series and E4R Series The cable between the Sensor and the Amplifier Unit (labeled as 1 below) must not be...
https://www.ia.omron.com/support/faq/answer/56/faq01281/