| Site Search | Product Search | IA Global Search |
... from 2 to 3 for the E5CC-T and from 3 to 4 for the E5EC-T/E5AC-T. Easier Numeric Inputs with a Digit Shift Key Digit shift: When setting the SP or other parameters, you can use a Sh...
...mmunications Data Communications format CompoWay/F 2-1-5 Set (monitor) Negative values values 8-digit hexadecimal 2's complement Decimal point Decimal point is removed and the result is conve...
...arm status.*1 put/alarm status.*1 put/alarm status.*1 remarks 01 hex 0: No decimal point 1: One digit decimal point Ch2 Decimal Point Position Monitor Decimal point position for Ch2. This dat...
...Manager then use the Fleet IP address for this parameter. • Select Call to increment the active digit. Select Next to select the next digit. After the last digit Next will a...
https://www.omron.com.au/data_pdf/mnu/i677-e-02_mobile_io_box.pdf
...nning on the Virtual Fleet Manager. For reference, the major version is determined by the first digit of the version number (e.g. 4.x.x). 1-1-2 FLOW Core Fleet Manager Renewal License FLOW Co...
https://www.omron.com.au/data_pdf/mnu/i695-e-01_virtualfleetmanager.pdf
...er. C. Press the S key in the monitor state to cause the product to enter the change state. • A digit that can be changed will start blinking. D. Use the S and U keys to change the set value....
...s. ax 4. 0000 Prescale AY ps. ay 10 03 Time unit time off Decimal point position dp ,,,,. , One digit below the decimal point Comparative output pattern out-p nomal Standard outputs Input Adj...
https://www.omron.com.au/data_pdf/mnu/n136-e1-08_k3hb-r_p_c.pdf
...d words in the CIO area. With Celsius selected: ±0.3% of PV or ±1ºC, whichever is greater, ±1 digit max. With Fahrenheit selected: ±0.3% of PV or ±2ºF, whichever is greater, ±1 ...
https://www.omron.com.au/data_pdf/mnu/p164-e1-03_cs1g_cs1h_cj2_replace.pdf
...red on (Racks 0 to 7) The number of Units detected on each Rack is Retained Cleared stored in 1-digit hexadecimal (0 to A hex).Rack 0: A336.00 to A336.03 Rack 1: A336.04 to A336.07 Rack 2: A3...
https://www.omron.com.au/data_pdf/mnu/p172-e1-01_cs_cj_practice.pdf
...ry M 1 C L K Manufactured after May 1996 The manufacturing date can be determined from the four-digit lot number on the side of the CPU Unit. Lot No.: @ @ 5 6: Manufactured in May 1996 Indica...
https://www.omron.com.au/data_pdf/mnu/w370-e1-07_cs1w-clk__(-v1)_cvm1-clk_2.pdf
...of digits 5 max. including sign and decimal point Numeric range –5000 to 99999 Example with one digit below the decimal point: –550.0 to 9999.9 Generate the CX-Process Plus tag file using the...
https://www.omron.com.au/data_pdf/mnu/w372-e1-16_cx-processtool.pdf
...ensation PID Compensation control 150 Accumulator for Accumulates analog signals, and outputs 8-digit instantaneous accumulated value signals. value input 151 CPU Unit Running Accumulates the...
https://www.omron.com.au/data_pdf/mnu/w374-03_cs1w-lc001.pdf
...ation PID control Accumulator for Accumulates analog signals, and instantaneous value outputs 8-digit accumulated value input signals. Run Time Accumulates the operating time, and Accumulator...
https://www.omron.com.au/data_pdf/mnu/w375-e1-05_cs1w-lc001.pdf
...four least significant digits and the most significant word (MSW) contains the most significant digit of the Indirect Address (refer to the examples on the following pages). Example Range Mod...
https://www.omron.com.au/data_pdf/mnu/w401-e1-06_cj1w-ct021.pdf
...OST RUN ERC SD RD LNK 0 0 Unit Number Switch Used to set the Ethernet Unit's unit number in one digit hexadecimal. 1 ×161 ×160 Node Address Switches Used to set the Ethernet Unit's FINS node ...
https://www.omron.com.au/data_pdf/mnu/w420-e1-06_cs1w_cj1w-etn21.pdf
...- - - - - - - - - - - - 03 02 01 00 TCP connection status The status is shown in bits 0 to 3 (1-digit hexadecimal), as follows: 112 Number 00000000 Status CLOSED Connection closed. Meaning 00...
https://www.omron.com.au/data_pdf/mnu/w421-e1-04_cs1w_cj1w-etn21.pdf
...play the operating status of the Unit. Unit Number Switch (page 30) Sets the unit number in one digit hexadecimal. Node Number Switches (page 31) Set the Unit’s FINS node number in two digits...
https://www.omron.com.au/data_pdf/mnu/w432-e1-01_cs1w-fln02_12.pdf
...l), Slave Unit type, and applicable node address (1-bit dot notation for the 100 position for 3-digit decimal) are alternately displayed (i.e., the cause of the error). Note The error codes a...
https://www.omron.com.au/data_pdf/mnu/w456-e1-04_cs1w_cj1w-crm21.pdf
...he sensor error.) Typical thermocouple inputs: (±0.3% of PV or ±1.5°C, whichever is greater) ±1 digit max. Special cases: • The accuracy of L is ±2°C ±1 digit max. • The accuracy of ...
https://www.omron.com.au/data_pdf/mnu/w466-e1-02_cj1w-ad04u(-sl).pdf
...ion Data attribute Index (hex) : This is the index of the NX object that is expressed as a four-digit hexadecimal number. Subindex (hex) : This is the subindex of the NX object that is expres...
https://www.omron.com.au/data_pdf/mnu/w524-e1-11_nx-ec0_ecs_pg.pdf