| Site Search | Product Search | IA Global Search |
... Sensor input Sensor input CIO 0.00 CIO 0.01 CIO 0.03 Reset input CIO 0.04 OK output CIO 100.00 NG output 1 CIO 100.01 NG output 2 CIO 100.02 NG output 3 CIO 100.03 ...
... EtherCAT Master to CPU Unit Data Set in 15 UINT Arrays from Ether- CAT Master to CPU Unit 1601 NG: The following shows the combination of the data sets with different names, and the data can...
https://www.omron.com.tw/data_pdf/mnu/w626-e1-01_nx-ect101.pdf
...pment Arrangement Control panel Control panel High-voltage power panel Controller Controller OK NG Arrangement of Controller and Units The coils and contacts in electromagnetic contacts and r...
https://www.omron.com.tw/data_pdf/mnu/w629-e1-08_nx502-1_00.pdf
...ng FTP 5 5-5-1 Steps for setting up FTP communications on the FHV7 Image logging settings: Only NG or All (If you select None, nothing will be saved to the NYE IPC.) Item Description Save Des...
https://www.omron.com.tw/data_pdf/mnu/w642-e2-01_nye2a-20f11-__wr1_00.pdf
... settings for the current adjustment will be cancelled and the display will change to LINER. OK NG 59 ZX-E Operation Manual Section 3 Adjusting Linearity Section 3 BASIC OPERATION Initializin...
...orrectly, the display will be [OK]. If scaling was unable to be completed, the display will be [NG]. Check that the sensing object is within the measurement range and execute scaling again. S...
...orkpiece 5-8 Simultaneous Logging Images and Measured Values for Multiple Controllers 5-11 Save NG Images for 1 Day 5-14 Logging of Images Before and After NG 5-16 Section 6 APPENDIX...
...d condition, number of triggers 1 to 100000 (times) 06h Interval of saving image 0: All 1: Save NG It is available only if [Save image] is set to ON. 07h NG save mode 0: OR 1: AND 02...
...nd. The command was executed properly: The command was not executed properly or the setting was NG: The delimiter can be selected from the following three types. CR/LF/CR+LF Space Delimiter M...
...tion 2 Part Names and Functions Judgment results/warning states and indicators OK: ON when PASS NG: ON whether other than PASS (HIGH or LOW) WARN: ON in warning state Peak-OK: ON when the pea...
...IC lead width judgment modes, both the HIGH and LOW outputs turn ON when the judgment result is NG. *2: In the IC lead pitch and IC lead width judgment modes, 0 V or 4 mA is output at all tim...
...operation result(Green/Red) READ/WRITE : READ or WRITE operation status(Green/Yellow) VERIFY OK/NG : Verify Read operation result(Green/Red) Data Display LED Date Display(Green) Error Code D...
https://www.omron.com.tw/data_pdf/mnu/z279-e1-09_v680-ham91_ham81.pdf
...s OK, and turns OFF when a setting is not made, measurement is OFF, the result of a judgment is NG, or an error occurs. (2) Laser indicator The laser indicator turns ON while the Sensor Head ...
.... . 31 Setting Logging Conditions . . . . . . . . . . . . . . . . . . . . 32 Logging Only at an NG/Only at an OK . . . . . . . . . . . . . 32 Logging by All Conditions . . . . . . . . . . . ....
https://www.omron.com.tw/data_pdf/mnu/z289-e1-03_zg2-dsu.pdf
...Page allows you to read and write data according to the command format of the Amplifier Unit OK/NG Display Area Page Designation Area Send Button Page/Write Designation Area Write Data Design...
https://www.omron.com.tw/data_pdf/mnu/z308-e1-02_v640-ham11-etn.pdf
...es to be judged as PASS by setting the HIGH and LOW thresholds. Press to display. Lit L HP 0 10 NG OK NG Press to set. [Change numeric value] [Move digit] Press to display. Lit Press...
...a The currently measured image and history of the overall judgement results (measurement count, NG count, and NG rate) will appear. Checking the Judgements of All Inspection Items in...
...operly if the object is not positioned inside this measurement region (e.g., the result will be NG even if the object is OK). In machines in which the position of the object varies for each i...
https://www.omron.com.tw/data_pdf/mnu/z329-e1-02_fq-cr1_____-m.pdf
...ollowed by
https://www.omron.com.tw/data_pdf/mnu/z353-e1-15_v680s-hmd6_-eip.pdf
...Page allows you to read and write data according to the command format of the Amplifier Unit OK/NG Display Area Page Designation Area Send Button Page/Write Designation Area Write Data Design...
https://www.omron.com.tw/data_pdf/mnu/z361-e1-08_v640-ham11(-l)-etn-v2.pdf