| Site Search | Product Search | IA Global Search |
...nsor. For example with the Through-beam type, the emitter is turned ON and OFF when there is no sensing object between the emitter and receiver. If the receiver does not turn ON and OFF accor...
...te product category Proximity Sensors The distance from the reference surface to the (standard) sensing object transit position that allows stable use, including the effects of temperature an...
...as Mark Sensors. Although these Sensors have fast response times, their drawbacks include short sensing distances and susceptibility to external light interference....
...ropriate product category Safety Sensors A function used in applications where a portion of the sensing area of a Safety Light Curtain is always interrupted by an object that mains stationary...
...F only if the total number of interrupted beams exceeds the set number of beams anywhere in the sensing area. The number of beams that can be set depends on the model of Safety Light Curtain....
...h light from the emitter is reflected by a Reflector before it is received by the receiver. The sensing object is positioned between the Photoelectric Sensor and the Reflector and when it int...
...s One of the modes of a Fiber Amplifier Unit, this mode provides the fastest response time. The sensing distance is the shortest....
...ate product category Photoelectric Sensors A Sensor in which light from the emitter strikes the sensing object and the light reflected from the sensing object enters the receiver, in...
... Definition The appropriate product category Safety Sensors Disabling detection for part of the sensing area....
... This function is used when a machine or workpiece constantly interrupts beams in a part of the sensing area and moves within the sensing area....
...otoelectric Sensors A Sensor that detects a position from the angle of light reflected from the sensing object to detect the presence or absence of the sensing object within a specif...
...r that detects leakage from facilities or machines, including various type of products, such as Sensing Bands, Point Sensors, Chemical-resistance Sensors, and Sensors resistant to high temper...
... of the modes of a Fiber Amplifier Unit, this mode provides more-precise detection and a longer sensing distance than standard mode....
... of a Fiber Amplifier Unit, this mode provides faster response time than the standard mode. The sensing distance is shorter than that of standard mode....
...tegory Ultrasonic Sensors The Ultrasonic Sensor sends ultrasonic waves from an emitter toward a sensing object, then receives the reflected waves with a receiver. The Sensor uses the resultin...
...ier that detects disconnections between the Leakage Sensor Amplifier and the end of the Leakage Sensing Band. When a disconnection is detected, an open-collector output is turned ON or OFF....
...lectric Sensors The diameter of the light beam from a Photoelectric Sensor where it strikes the sensing object....
...element. Modulated light: Method used to detect light emitted in pulses by the emitter element. Sensing distance Through-beam Sensors (with slot) The slot width, i.e., the distance between th...
https://www.ia.omron.com/support/guide/24/explanation_of_terms.html
...lated Contents Related Contents Proximity Sensors Products Cautions Primary Contents Standard Sensing Object A sensing object that serves as a reference for measuring basic perform...
https://www.ia.omron.com/support/guide/41/explanation_of_terms.html
...nts Photoelectric Sensors Products Cautions Primary Contents Item Explanatory diagram Meaning Sensing distance Through- beam Sensors The maximum sensing distance that can be set wi...
https://www.ia.omron.com/support/guide/43/explanation_of_terms.html