| Site Search | Product Search | IA Global Search |
... If the input is connected to a UPS, do not connect a UPS with a square-wave output. Doing so will cause the internal temperature of the product to increase, possibly causing smokin...
https://www.omron-ap.com.ph/products/family/3821/specification.html
...32-LD11 2M 860 360 250 110 E32-LD11R 2M 840 350 240 100 * The fiber length is 2 m on each side, so the sensing distance is given as 4,000 mm. Cylindrical Models Sensing method Size Sensing di...
https://www.omron-ap.com.ph/products/family/3831/specification.html
...d in continuous or strobed mode. NERLITE Smart Series Lights have a built-in strobe controller, so no external strobe controller is needed. Dedicated cable sets allow you to wire the NERLITE ...
https://www.omron-ap.com.ph/products/family/3847/lineup.html
...AC G2RV-ST700/500-AP 230 VAC Note: Voltage is reduced within the socket for the slim I/O relay, so the rated input voltage and rated coil voltage of replacement relays are different. Accessor...
https://www.omron-ap.com.ph/products/family/3868/lineup.html
...ld be 1 to 5 mm. Note: 2. To allow easier operation, it is recommended that Adapters be mounted so that the gap between sides with hooks is at least 15 mm (i.e., with the panel cutouts separa...
https://www.omron-ap.com.ph/products/family/3899/dimension.html
...tal Filter This function sets the time constant applied to the first-order lag operation filter so that the noise components mixed with the measured value are eliminated. All models Measuring...
https://www.omron-ap.com.ph/products/family/3902/specification.html
...nd the wire 4 turns due to the limitation of the wire size, decrease the number to 3, 2, and so on. When the wire can be wound only a single turn, use 4 or more filters side by side, wi...
https://www.omron-ap.com.ph/products/family/3912/specification.html
... Safety Sensors E3ZS OMRON Non-contact Safety Door Switches D40A-2, D40A Safety Output Units NX-SO Unit type Appearance Specifications Unit version Model Number of safety output points Intern...
https://www.omron-ap.com.ph/products/family/3920/lineup.html
...before attempting a megger test (insulation resistance measurement) on a Servo Drive. Not doing so may result in the Servo Drive failure. Do not perform a dielectric strength test on the Serv...
https://www.omron-ap.com.ph/products/family/3923/specification.html
...value (peak hold), the bottom value (bottom hold), the range of change (peak-to-peak hold), and so forth. Timer mode Allows you to delay upon changes in judgment output, or turn PASS output O...
https://www.omron-ap.com.ph/products/family/3932/specification.html
...rection. (Maintain the specified mounting space between Controllers.) • To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. • When two or more...
https://www.omron-ap.com.ph/products/family/3937/dimension.html
...rection. (Maintain the specified mounting space between Controllers.) • To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. • When two or more...
https://www.omron-ap.com.ph/products/family/3938/dimension.html
...A switched and 10 A safe switched are from the same source and pass through the same 10 A fuse, so the sum of their current must be less than 10 A. Standards AMR EN IS0 12100, EN ISO 13849-1,...
https://www.omron-ap.com.ph/products/family/3950/specification.html
...nnector. *3. However, when bending the cable to perform wiring, maintenance, and other work, do so within the temperature range of 0 to 75°C in consideration of severing of the cable. last up...
https://www.omron-ap.com.ph/products/family/871/specification.html
...rection. (Maintain the specified mounting space between Controllers.) • To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. • When two or more...
https://www.omron-ap.com/products/family/1434/dimension.html
...s, Ltd. --- * There is a risk of quality problems when using cables assembled by typical users, so we recommend purchasing cables with preattached connectors or having a qualified technici...
...tch a standard load, it cannot be used for a load of a smaller capacity. Doing so may result in roughening of the contact surface and contact reliability may be lost. *1. The...
https://www.omron-ap.com/products/family/1497/specification.html
...tch a standard load, it cannot be used for a load of a smaller capacity. Doing so may result in roughening of the contact surface and contact reliability may be lost. *1. The...
https://www.omron-ap.com/products/family/1498/specification.html
...V E39-F1V E32-T84SV 1M (No Cutting) E32-T10V 2M (Free Cutting) E32-VF4 Note 1. Mount the Flange so that the V40 O-ring is on the atmospheric-pressure side of the vacuum chamber wall. Note 2. ...
https://www.omron-ap.com/products/family/1532/dimension.html
...,000 * HS: 3,450 ST: 4,000 * SHS: 920 E32-LT11R 2M * The optical fiber is 2m long on each side, so the sensing distance is 4,000 mm. Note 1. The following mode names and response times apply ...