| Site Search | Product Search | IA Global Search |
...lue is calculated from the difference between the heights of the surface and rear surface, so there is no effect on the temperature change. ZW-S7010/S7020/S7030/S7040/SP7007/SP7010/SPR70...
https://www.omron.co.id/products/family/3500/specification.html
...before attempting a megger test (insulation resistance measurement) on a Servo Drive. Not doing so may result in the Servo Drive failure. Do not perform a dielectric strength test on the Serv...
https://www.omron.co.id/products/family/3549/specification.html
...32, 64 or 96 GB 8, 16, 32, 64 GB Memory type DDR4 (ECC is available) DDR4 Package Memory Format SO-DIMM Serial Presence Detect (SPD) Speed grade 3200 MT/s CAS latency CL17 Trusted platform mo...
https://www.omron.co.id/products/family/3631/specification.html
...ion minimal 10yr) Memory Memory size *1 8, 16, 32, 64 GB Memory type DDR4 Package Memory Format SO-DIMM Serial Presence Detect (SPD) Speed grade 3200 MT/s CAS latency CL17 Trusted platform mo...
https://www.omron.co.id/products/family/3633/specification.html
...ally, turn OFF all of the pins. C SD Memory Card power supply switch Turns OFF the power supply so that you can remove the SD Memory Card. D DIN Track mounting hook These hooks are used to mo...
https://www.omron.co.id/products/family/3650/specification.html
...cteristics of fuses and the operating characteristics of breakers and select fuses and breakers so that external fuses will not burn out or breakers will not operate due to inrush current. Ri...
https://www.omron.co.id/products/family/3656/specification.html
...ection. (Main-tain the specified mounting space between Controllers.) • To mount the Controller so that it is waterproof, insert the water-proof packing onto the Controller. • When two or mor...
...irection. (Maintain the specified mounting space between Controllers.) •To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. •When two or more ...
...ection. (Main-tain the specified mounting space between Controllers.) • To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. • When two or more...
...rection. (Maintain the specified mounting space between Controllers.) • To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. • When two or more...
...chment is used. *6. Even if the motor is not moving, the value of velocity may appear slightly, so that the measurement value is fixed at 0.00 mm/s until the value reaches 0.90 mm/s or h...
https://www.omron.co.id/products/family/3686/specification.html
...ning. If the input is connected to a UPS, do not connect a UPS with a square-wave output. Doing so will cause the internal temperature of the product to increase, possibly causing smoking or ...
https://www.omron.co.id/products/family/3687/specification.html
...2 *1. If the input is connected to a UPS, do not connect a UPS with a square-wave output. Doing so will cause the internal temperature of the product to increase, possibly causing smok...
https://www.omron.co.id/products/family/3688/specification.html
...32-LD11 2M 820 330 250 74 E32-LD11R 2M 790 310 240 71 *1. The fiber length is 2 m on each side, so the sensing distance is given as 4,000 mm. Cylindrical Models Sensing method Size Sensing di...
https://www.omron.co.id/products/family/3694/specification.html
...tal Filter This function sets the time constant applied to the first-order lag operation filter so that the noise components mixed with the measured value are eliminated. All models Measuring...
https://www.omron.co.id/products/family/3699/specification.html
...e theme on both the piping side and the sensor mounting side. Because the sensor is designed so that the measurement area is in the center of the piping, correct measurement may not be ...
.... Z405). Note: 2. Do not connect the Conversion Cable for the following purposes. Failure to do so may result in failure. 1. Connecting with the F39-SGIT-IL3, F39-GCNY2, F39-GCNY...
...If the input is connected to a UPS, do not connect a UPS with a square-wave output. Doing so will cause the internal temperature of the product to increase, possibly causing smoki...
https://www.omron.co.id/products/family/3753/specification.html
... test (insulation resistance measurement) on a Servo Drive. Not doing so may result in the Servo Drive failure. Do not perform a dielectric strength tes...
https://www.omron.co.id/products/family/3776/specification.html
...mA max. Note: 1. Alarm signal output is not equipped with an internal current limiting circuit, so be sure that the current flowing to the alarm signal output terminals does not exceed 50 mA....
https://www.omron.co.id/products/family/3780/specification.html