| Site Search | Product Search | IA Global Search |
...irection. (Maintain the specified mounting space between Controllers.) •To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. •When two or more ...
https://www.omron.com.vn/products/family/3669/dimension.html
...ection. (Main-tain the specified mounting space between Controllers.) • To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. • When two or more...
https://www.omron.com.vn/products/family/3671/dimension.html
...rection. (Maintain the specified mounting space between Controllers.) • To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. • When two or more...
https://www.omron.com.vn/products/family/3672/dimension.html
...chment is used. *6. Even if the motor is not moving, the value of velocity may appear slightly, so that the measurement value is fixed at 0.00 mm/s until the value reaches 0.90 mm/s or h...
https://www.omron.com.vn/products/family/3686/specification.html
...ning. If the input is connected to a UPS, do not connect a UPS with a square-wave output. Doing so will cause the internal temperature of the product to increase, possibly causing smoking or ...
https://www.omron.com.vn/products/family/3687/specification.html
...2 *1. If the input is connected to a UPS, do not connect a UPS with a square-wave output. Doing so will cause the internal temperature of the product to increase, possibly causing smok...
https://www.omron.com.vn/products/family/3688/specification.html
...32-LD11 2M 820 330 250 74 E32-LD11R 2M 790 310 240 71 *1. The fiber length is 2 m on each side, so the sensing distance is given as 4,000 mm. Cylindrical Models Sensing method Size Sensing di...
https://www.omron.com.vn/products/family/3694/specification.html
...tal Filter This function sets the time constant applied to the first-order lag operation filter so that the noise components mixed with the measured value are eliminated. All models Measuring...
https://www.omron.com.vn/products/family/3699/specification.html
...e theme on both the piping side and the sensor mounting side. Because the sensor is designed so that the measurement area is in the center of the piping, correct measurement may not be ...
.... Z405). Note: 2. Do not connect the Conversion Cable for the following purposes. Failure to do so may result in failure. 1. Connecting with the F39-SGIT-IL3, F39-GCNY2, F39-GCNY...
...If the input is connected to a UPS, do not connect a UPS with a square-wave output. Doing so will cause the internal temperature of the product to increase, possibly causing smoki...
https://www.omron.com.vn/products/family/3753/specification.html
... test (insulation resistance measurement) on a Servo Drive. Not doing so may result in the Servo Drive failure. Do not perform a dielectric strength tes...
https://www.omron.com.vn/products/family/3776/specification.html
...mA max. Note: 1. Alarm signal output is not equipped with an internal current limiting circuit, so be sure that the current flowing to the alarm signal output terminals does not exceed 50 mA....
https://www.omron.com.vn/products/family/3780/specification.html
...4GS-NK4 Note 1. When determining the operation key insertion radius, adjust the adjusting screw so that the tip of the operation key is positioned to the center of the key insert...
...s should be 1 to 5 mm. 2. To allow easier operation, it is recommended that Adapters be mounted so that the gap between sides with hooks is at least 15 mm (i.e., with the panel cutouts separa...
https://www.omron.com.vn/products/family/3809/dimension.html
...s should be 1 to 5 mm. 2. To allow easier operation, it is recommended that Adapters be mounted so that the gap between sides with hooks is at least 15 mm (i.e., with the panel cutouts separa...
https://www.omron.com.vn/products/family/3810/dimension.html
... If the input is connected to a UPS, do not connect a UPS with a square-wave output. Doing so will cause the internal temperature of the product to increase, possibly causing smokin...
https://www.omron.com.vn/products/family/3821/specification.html
...32-LD11 2M 860 360 250 110 E32-LD11R 2M 840 350 240 100 * The fiber length is 2 m on each side, so the sensing distance is given as 4,000 mm. Cylindrical Models Sensing method Size Sensing di...
https://www.omron.com.vn/products/family/3831/specification.html
...d in continuous or strobed mode. NERLITE Smart Series Lights have a built-in strobe controller, so no external strobe controller is needed. Dedicated cable sets allow you to wire the NERLITE ...
...AC G2RV-ST700/500-AP 230 VAC Note: Voltage is reduced within the socket for the slim I/O relay, so the rated input voltage and rated coil voltage of replacement relays are different. Accessor...