Site Search | Product Search | IA Global Search |
... round flag D4: RD0 Read signal D3 to D0:CS signals (CS3 to CS0) First Result Word: D15 to D12: Digit 4 D11 to D08: Digit 3 D07 to D04: Digit 2 D03 to D00: Digit 1 ...
https://www.omron-ap.com/data_pdf/mnu/p087-e1-03_cqm1_cqm1h_cj2m_replace.pdf
...d words in the CIO area. With Celsius selected: ±0.3% of PV or ±1ºC, whichever is greater, ±1 digit max. With Fahrenheit selected: ±0.3% of PV or ±2ºF, whichever is greater, ±1 ...
https://www.omron-ap.com/data_pdf/mnu/p164-e1-02_cs1g_cs1h_cj2_replace.pdf
...Control word C1 settings (C1: CIO 5010) Word Description (data type) Communications port No. (1 digit hex) Serial port No. (1 digit hex) C1 Unit address of destination device (2...
...ither from RAM or EEPROM and displays to the set value. Parameter No.: 0xxx(when the high order digit is 0) reads from the RAM area. 1xxx(when the high order digit is 1) reads from t...
https://www.omron-ap.com/data_pdf/mnu/v087-e1-01_ns5_ns8_ns10_ns12-v1_refer.pdf
...ntage to the rated torque of the motor. Servo Drive Unit Version 1.0 and 1.1 do not use decimal digit resolution, whereas Servo Drive Unit Version 1.2 or later uses 1 decimal digit r...
https://www.omron-ap.com/data_pdf/mnu/v453-e1-01_nx701_nj_01_na5-_w.pdf
...CD 4-byte integer BCD1 (Signed 1-WORD, Convert the data type with the PLC program highest-order digit is F) format for because the signed BCD integer is BCD2 (Signed 1-WORD, functional unavai...
https://www.omron-ap.com/data_pdf/mnu/v469-e1-04_ns_na_replace.pdf
...cessary Manufactured after May 1996 Note The manufacturing date can be determined from the four-digit lot number on the side of the CPU Unit. Lot No.: @ @ 5 6 . . . . . Manufactured in May 19...
https://www.omron-ap.com/data_pdf/mnu/w309-e1-12_c_1w_c200hw_cvm1_cqm1h-clk_cs1w-rpt.pdf
...sion including N) when using C200HX/HG/HE-series PLCs. Note Reads bits 0 to 11 of the word as 3-digit BCD. When using CS/CJseries PLCs, the bits are read as binary data. There are three types...
https://www.omron-ap.com/data_pdf/mnu/w344-e1-18_cx-protocol.pdf
...ations when an error occurs Two LED indicators (2 colors): Display Unit and network status. Two-digit 7-segment display: Displays the DeviceNet Unit node address, error code, and node address...
https://www.omron-ap.com/data_pdf/mnu/w380-e1-10_cs1w_cj1w-drm.pdf
... network to be connected to. • Node: The FINS network address and FINS node address. (The third digit is always 0.) • Unit: The FINS network address, FINS node address, and unit number of the...
https://www.omron-ap.com/data_pdf/mnu/w382-e1-04_ws02-3g8f5_3g8e2.pdf
...iled information First byte Communications cycle time set in the data link table (ms units, two-digit hexadecimal) Second byte Minimum communications cycle time that can be set (ms units, two...
https://www.omron-ap.com/data_pdf/mnu/w390-01_3g8f7-slk11-e_21-e.pdf
...or for instantaneous value input Run Time Accumulator Accumulates analog signals, and outputs 8-digit accumulated value signals. Time Sequence Data Statistics Records time sequence data from ...
https://www.omron-ap.com/data_pdf/mnu/w406-e1-10_cs1w-lcb_cs1d-cpu_cs1g-cpu.pdf
...s. In other words, for each 4 bits, the sum of ON bits are calculated and expressed as a single digit. MSB (Most Significant Bit) LSB (Least Significant Bit) Bit 15 14 13 12 11 10 09 08 07 06...
https://www.omron-ap.com/data_pdf/mnu/w461-e1-06_cp1l_cp1e.pdf
...he node number on the left will be grayed out and the node number will be the least-significant digit of the IP address of the computer at that time. Clear this selection to enable using an I...
https://www.omron-ap.com/data_pdf/mnu/w464-e1-15_cx-integrator.pdf
... specified word. { { 2-114 MOVE BIT MOVB/ @MOVB 082 Transfers the specified bit. { { 2-117 MOVE DIGIT MOVD/ @MOVD 083 Transfers the specified digit or digits. (Each digit is...
https://www.omron-ap.com/data_pdf/mnu/w483-e1-08_cp1e_cp2e.pdf
...efreshed during overseeing processing. Use PRV(881) to read the most recent PVs. Data format: 8 digit hexadecimal • Linear mode: 8000 0000 to 7FFF FFFF hex 0000 0000 to FFFF FFFF hex (for inc...
https://www.omron-ap.com/data_pdf/mnu/w486-e1-02_cj2m-cpu_-md21_.pdf
...ometer input: (Sensor error is not included.) (±0.3% of PV or ±0.8 °C, whichever is greater) ±1 digit max. Thermocouple input: (±0.3% of PV or ±1.5 °C, whichever is greater) ±1 digit...
https://www.omron-ap.com/data_pdf/mnu/w498-e1-03_cj1w-pdc15_ph41u_ad04u.pdf
...ion Data attribute Index (hex) : This is the index of the NX object that is expressed as a four-digit hexadecimal number. Subindex (hex) : This is the subindex of the NX object that is expres...
...herNet Unit that is mounted on the PLC that serves as a relay node. Node Address Enter the last digit of the IP address of the computer. (Example: 1 if the IP address is 192.168.250.1) Remote...
https://www.omron-ap.com/data_pdf/mnu/w570-e1-10_io-link_system.pdf
...t Unit that is mounted on the CPU Unit that serves as a relay node. Node Address Enter the last digit of the IP address of the computer. (Example: 1 if the IP address is 192.168.250.1) Remote...
https://www.omron-ap.com/data_pdf/mnu/w585-e1-03_cxone-al__d-v4.pdf