Site Search | Product Search | IA Global Search |
...he node number on the left will be grayed out and the node number will be the least-significant digit of the IP address of the computer at that time. Auto-detect Selection cleared. Clear this...
https://www.omron.com.tw/data_pdf/mnu/w464-e1-15_cx-integrator.pdf
... the specified word. {{2-114 MOVE BIT MOVB/ @MOVB 082 Transfers the specified bit. {{2-117 MOVE DIGIT MOVD/ @MOVD 083 Transfers the specified digit or digits. (Each digit is...
https://www.omron.com.tw/data_pdf/mnu/w483-e1-08_cp1e_cp2e.pdf
...efreshed during overseeing processing. Use PRV(881) to read the most recent PVs. Data format: 8 digit hexadecimal •Linear mode: 8000 0000 to 7FFF FFFF hex 0000 0000 to FFFF FFFF hex (for incr...
https://www.omron.com.tw/data_pdf/mnu/w486-e1-02_cj2m-cpu_-md21_.pdf
...le for CJ-series Unit.) Indication accuracy Centigrade:±0.3% PV or±1°C (whichever is larger)± 1 digit max. Fahrenheit:±0.3% PV or±2°F (whichever is larger)±1 digit max. •The accuracy...
https://www.omron.com.tw/data_pdf/mnu/w491-e1-03_cj1w-tc003_004_103_104.pdf
...nverted from ASCII to hexadecimal and stored here. Response code (4 digits Hex) Receive data (4-digit Hex) Send Data Allocation (SrcDat [ ] of ExecPMCR instruction) Receive Data Allocation (D...
https://www.omron.com.tw/data_pdf/mnu/w494-e1-04_cj1w-scu_2.pdf
...and the overall network. a. Two status indicators (two-color: Green or red indicators) b. A two-digit, 7-segment indicator c. Two dot indicators 2-1-1 Nomenclature and Functions CJ1W-DRM21 In...
https://www.omron.com.tw/data_pdf/mnu/w497-e1-03_cj1w-drm21.pdf
...- ion Data attri- bute Name Description Index (hex) The index of the NX object expressed by a 4-digit hexadecimal number. Subindex (hex) The subindex of the NX object expressed by a 2-...
...e exceeds the specified resolution of the relevant model, so use this value as reference data. •Digit data lost in conversion is rounded off. (Example) REAL data type of 1.454C •INT data for...
https://www.omron.com.tw/data_pdf/mnu/w566-e1-06_nx-ts_hb.pdf
...n Data attrib- ute Index (hex) : This is the index of the NX object that is expressed as a four-digit hexadecimal number. Subindex (hex) : This is the subindex of the NX object that is expres...
...r- Net Unit that is mounted on the PLC that serves as a relay node. Node Address Enter the last digit of the IP address of the computer. (Exam- ple: 1 if the IP address is 192.168.250.1) Remo...
https://www.omron.com.tw/data_pdf/mnu/w570-e1-10_io-link_system.pdf
...t Unit that is mounted on the CPU Unit that serves as a relay node. Node Address Enter the last digit of the IP address of the computer. (Example: 1 if the IP ad- dress is 192.168.250.1) Remo...
https://www.omron.com.tw/data_pdf/mnu/w585-e1-03_cxone-al__d-v4.pdf
...r of the Sysmac Studio. When the automatic generation method is selected, the least significant digit of the IP address is set as the FINS node address. When the combination or IP address met...
https://www.omron.com.tw/data_pdf/mnu/w596-e1-06_nx701_nx502_nx102.pdf
...] ReadData[3] 11 22 33 44 Address Memory address Data size RF Tag memory 11 22 33 44 CRC (Upper digit) CRC (Lower digit) 7bit 0bit : : 01 N Read target area Check code area (2 bytes)...
https://www.omron.com.tw/data_pdf/mnu/w609-e1-02_sysmac-xr019.pdf
...th the CX- ConfiguratorFDT 11 11-2-10 Going Online Item Description Node Address Enter the last digit of the IP address of the computer. (Example: 1 if the IP address is 192.168.250.1) Remote...
https://www.omron.com.tw/data_pdf/mnu/w619-e1-06_nxr-ilm08c-eit.pdf
...one byte. A single byte of data can be written to one address. to Address Data Most significant digit Least significant digit 1 byte Production date area Write protect setting area 2...
https://www.omron.com.tw/data_pdf/mnu/z129-e1-02_v600-ham42-drt.pdf
...or 4 "02" MRC 2 SRC 2 Response code 4 "01" Write data length No. of elements For double-word (8-digit) variable type 24 max. (0018H) For word (4-digit) variable type 48 max. (0030H) ...
...otary switches are used to set the CompoNet node address. The left rotary switch sets the ten's digit, and the right rotary switch sets the one's digit. Set the Unit’s Com- poNet nod...
...Antenna) 9 - Do not set. (A mode setting error will occur.) Item Description Setting method Two-digit decimal number The left rotary switch sets the 10s digit, and the right rotary s...
https://www.omron.com.tw/data_pdf/mnu/z278-e1-10_v680-ham42-drt.pdf
...ange for each channel using the keys, and press the SET key to apply the setting. The uppermost digit is displayed on a white background. Irradiation power (%) Irradiation time (s) CH1 Irradi...
...e the text string "2014/01/01," enter "2014/01/01" in the string format area. To recognize four-digit numbers, enter as [####], where each "#" represents a number, in the string format area. ...
https://www.omron.com.tw/data_pdf/mnu/z337-e1-12_fq2-s_ch.pdf