Site Search | Product Search | IA Global Search |
...リガのレベルです。 この値を内部トリガソースとなる特徴量が超えたとき、 トリガ点となります。 H'8007 ∼ H'7FF9(-32761 ∼ 32761[digit]) 初期値:H'7FF9(32761[digit]) 即時 H'0103 内部ト...
...ata update Details cycle 5 ms Measurement accuracy: ±2% (percentage of output voltage value) ±1 digit 5 ms Measurement accuracy: ±5% (percentage of rated output current) ±1 digit 5 m...
https://www.fa.omron.co.jp/data_pdf/mnu/t213-e1-07_s8vk-x.pdf
...rganization of the Manual, and How to Use It: The related manuals are listed below. * The final digit of the manual number is the revision code. For operating the Support Tool S NT-series Sup...
https://www.fa.omron.co.jp/data_pdf/mnu/v061-e1-06_nt-zjcmx1-v4.pdf
...NT31/NT31C Thumbwheel Switches Numeric values can be input by incrementing or decrementing each digit with the corresponding touch switch (+, –). The input numeric values can also be stored i...
https://www.fa.omron.co.jp/data_pdf/mnu/v062-e1-06_nt31_31c_setup.pdf
...631/NT631C Thumbwheel Switches Numeric values can be input by incrementing or decrementing each digit with the corresponding touch switch (+, –). The input numeric values can also be stored i...
https://www.fa.omron.co.jp/data_pdf/mnu/v063-e1-05_nt631_631c_setup.pdf
...m Word m+1 14 13 12 11 10 9 8 Bit 7 6 5 4 3 2 1 Numeral/character string memory table number (4-digit BCD or hexadecimal) PT status notify bits 0 0 0 Word 15 Word m 0 14 13 12 11 10 9 8 7 6 5...
https://www.fa.omron.co.jp/data_pdf/mnu/v066-01_nt-drt21.pdf
...NT31 NT631 Thumbwheel Switches Numeric values can be input by incrementing or decrementing each digit with the corresponding touch switch (+, –). The input numeric values can also be stored i...
https://www.fa.omron.co.jp/data_pdf/mnu/v069-e1-03_nt21_nt31_nt631.pdf
...ither from RAM or EEPROM and displays to the set value. Parameter No.: 0xxx(when the high order digit is 0) reads from the RAM area. 1xxx(when the high order digit is 1) reads from t...
https://www.fa.omron.co.jp/data_pdf/mnu/v087-e1-01_ns5_ns8_ns10_ns12-v1_refer.pdf
...le generation year/month/day]: YYYYMMDD • [file generation hour/minute]: hhmm*1 *2 • [index]: 3-digit serial number (default: 000) Duplicate values are incremented by “1”. *1. Fixed at “0000”...
https://www.fa.omron.co.jp/data_pdf/mnu/v118-e1-25_na5-______.pdf
...E in hex (1 to 126 in decimal). Setting range 01 to 7E (1 to 126 in decimal) 16 1 Set the upper digit using the top rotary switch and the lower digit using the bottom rotary switch. ...
https://www.fa.omron.co.jp/data_pdf/mnu/v119-e1-15_na5-______.pdf
...ctive Flag (Not used) 13 12 (Not used) (Not used) 11 10 Startup Mode (hexadecimal: 1 0: Stopped digit) 1: User set 2: Automatically set 3: Status monitor (Board not participating in data link...
https://www.fa.omron.co.jp/data_pdf/mnu/v228-e1-02_itnc-epx-drm.pdf
...ame Unit number switch (UNIT NO.) Function Sets the unit number of the SYSMAC SPU Unit as a one-digit hexadecimal value. Do not set the same unit number for more than one CPU Bus Unit under t...
... Pitch Angle(β) ±30° Tilt Angle(γ) ±25° Reading of bar-codes on curved surface(R) R≧ 20mm(UPC12 digit) Light source Red Laser Diode (Wave Length : 650nm) Light Output 1.0mW or less Scan Type ...
https://www.fa.omron.co.jp/data_pdf/mnu/v500-r2cf_inst-5339935-0h.pdf
...ss Check code calculation area (no. of check bytes − 2) No. of area bytes Check area CRC (upper digit) CRC (lower digit) Check code area (2 bytes) Note The last two bytes of a check ...
https://www.fa.omron.co.jp/data_pdf/mnu/w153-e1-04_c200h-ids.pdf
...H5E &HBF4 Floating Point Constants Single precision: This type of constant is stored with seven-digit precision and is output as a six-digit constant with the seventh digit ...
https://www.fa.omron.co.jp/data_pdf/mnu/w165-e1-04_c200h_asc02.pdf
... number switches. Node number switches determine the node number. The left switch sets the tens digit; the right switch sets the ones digit. The node number must be between 01 and 62...
https://www.fa.omron.co.jp/data_pdf/mnu/w174-e1-07_c200hw_slk___c1000h_slk__-v1.pdf
...e following lot number or later support the following new functions. 01 Z 4 0 Year (1994): Last digit of the Christian year Month (December): (9: September, X: October, Y: November, X: Decemb...
https://www.fa.omron.co.jp/data_pdf/mnu/w225-e1-05_c200h-tc.pdf
...ow has been added to products with the following lot number and later ones. 07 Z 4 O 1994 (last digit of the year) December (X: October, Y: November, Z: December) 07 (7th day of the month) De...
https://www.fa.omron.co.jp/data_pdf/mnu/w241-e1-03_c200h-pid.pdf
...d the status of communications with the Slaves. Rotary Switch This switch sets the Master's one-digit hexadecimal unit number. DIP Switch These pins have the following functions: Pin 1: Usabl...
https://www.fa.omron.co.jp/data_pdf/mnu/w266-e1-09_c200hw_cj1w_cqm1_srt1_srt2.pdf
...areas by word, all that is necessary is the acronym (if required) and the two-, three-, or four-digit word address. To designate an area by bit, the word address is combined with the bit numb...
https://www.fa.omron.co.jp/data_pdf/mnu/w303-e1-09_c200hx_hg_he_ope.pdf