| Site Search | Product Search | IA Global Search |
...surement value to the set value, which makes it easy to understand the status. Three indicators light up when the status reaches 50% All indicators light up when the status reaches 1...
https://www.omron.com.tw/data_pdf/cat/h3_h5_timer_selection_guide_l130-e1_2_1_csm1129246.pdf
... case examples for each individual model Page: E-1 21 Operation not displayed. Display does not light even if power is supplied. Internal circuit is damaged. Check the polarity of the pow- er...
https://www.omron.com.tw/data_pdf/mnu/c154-e1-02_limit-switches_tg.pdf
...en operation starts. Standard Models After the power comes ON, all indicators and displays will light for approximately 1 second, and then the operation display will appear. The top display w...
...ining slaves. For a Mitsubishi PLC, the ERR. indicator on the Serial Communications Module will light during the copying process, but this does not indicate an error. The ERR. indicator will ...
...D medium and large scanners are Class 3R or Class 2 laser devices. •Avoid eye exposure to laser light. Looking at the laser beam may cause injury to the retina. When accidental eye exposure i...
... the correct direction. “PC”will flash on the seven-segment display and the card indicator will light when the PC card can be used. 3. Place the card holder on the PC card and tighten the scr...
https://www.omron.com.tw/data_pdf/mnu/v236-e1-04_cs1w-spu0_-v2_cj1w-spu01-v2.pdf
...ables use quartz-glass fibers with a hard-clad coating (hard acrylic fluoride plastic) to carry light signals. Optical signals travel through the glass fiber for distances up to 1 km. Though ...
https://www.omron.com.tw/data_pdf/mnu/w156-03_s3200-hcc_hcl.pdf
...Error Code; and the se- quence number and I/O status of each axis are shown under Status. A red light indicates that an I/O signal is ON. For error details, refer to the relevant Position Con...
https://www.omron.com.tw/data_pdf/mnu/w433-e1-10_cx-position.pdf
...surement value to the set value, which makes it easy to understand the status. Three indicators light up when the status reaches 50% All indicators light up when the status reaches 1...
https://www.omron.com.vn/data_pdf/cat/h3_h5_timer_selection_guide_l130-e1_2_1_csm1129246.pdf
...data it contains. Precautions during Memory Card Access The BUSY indicator on the CPU Unit will light when the Memory Card is being accessed. 1. Never turn OFF the power to the PLC while the ...
https://www.omron.com.vn/data_pdf/cat/hmc-ef183_ds_e_3_2_csm1609.pdf
...harden and crack, resulting in the ingress of cutting oil into the fiber core. This reduces the light level. Cutting oil The fluororesin that covers the entire surface of the cable sheath (fi...
https://www.omron.com.vn/data_pdf/cat/oil-resistant_components_y215-e1_6_6_csm1053244.pdf
...ating equipment. Places subject to splashing liquid or oil atmosphere. Places subject to strong light, such as direct sunlight, fluorescent light, or incandescent light. Pla...
...set an output assignment to alarm 1. After the power comes ON, all indicators and displays will light for approximately 1 second, and then the operation display will appear. The top display w...
...ining slaves. For a Mitsubishi PLC, the ERR. indicator on the Serial Communications Module will light during the copying process, but this does not indicate an error. The ERR. indicator will ...
... user terminal, an executing program, or a pendant. Once this request has been made, the button light blinks, and the operator must press the button for high power to be applied. The default ...
https://www.omron.com.vn/data_pdf/mnu/i602-e-03_smartcontroller_ex.pdf
...the correct direction. “PC” will flash on the seven-segment display and the card indicator will light when the PC card can be used. 3. Place the card holder on the PC card and tighten the scr...
https://www.omron.com.vn/data_pdf/mnu/v236-e1-04_cs1w-spu0_-v2_cj1w-spu01-v2.pdf
...ables use quartz-glass fibers with a hard-clad coating (hard acrylic fluoride plastic) to carry light signals. Optical signals travel through the glass fiber for distances up to 1 km. Though ...
https://www.omron.com.vn/data_pdf/mnu/w156-03_s3200-hcc_hcl.pdf
..., CJ1-H, and CJ1M CPU Units are backed up in the built-in flash memory. The BKUP indicator will light on the front of the CPU Unit when the backup operation is in progress. Do not turn OFF th...
https://www.omron.com.vn/data_pdf/mnu/w394-e1-16_cs_cj_nsj.pdf
...r Error Code; and the sequence number and I/O status of each axis are shown under Status. A red light indicates that an I/O signal is ON. For error details, refer to the relevant Position Con...
https://www.omron.com.vn/data_pdf/mnu/w433-e1-10_cx-position.pdf
...setting method for the CS1W-FLN22 or CJ1W-FLN22, a setting error will occur (HER indicator will light). Set the IP address setting method to either 192.168.250 + node No. (default) or Setup A...
https://www.omron.com.vn/data_pdf/mnu/w440-e1-04_cj1w_cs1w-fln.pdf