| Site Search | Product Search | IA Global Search |
...d in continuous or strobed mode. NERLITE Smart Series Lights have a built-in strobe controller, so no external strobe controller is needed. Dedicated cable sets allow you to wire the NERLITE ...
...• The Configurator can be used to calibrate temperatures. • The circuit section can be removed, so rewiring isn’t required during maintenance. • DIN track mounting. last update: December 19, ...
...inescent color of the LED. The materials used for the IP40 and oil-resistant IP66 are different so be sure to use a Color Cap that matches the specifications of the Switch. • Not all combinat...
... be replaced during power supply or operation. In addition, cable disconnections are monitored, so failures can be located easily. Remove or add units without using a programming device The d...
...DS10T-V. Meanwhile, the ZX-TDS10T-VL can control air push models in addition to air lift models so that contact force can now be controlled externally. Combines Reliability and Innovations in...
...he 0.5-m type, a repeat accuracy of 1 mm or better has been achieved. The Sensor is ultrasonic, so it is not affected by the color of objects. A variety of materials can be measured, includin...
...nits by making a hole in the bracket and tightening just one nut. • The cable follows the wall, so extra space is not required, and the cable will not get caught on other objects. A Fiber Uni...
... UDP/IP are supported, in addition to FINS messages, FTP file transfers, and mail notification, so that production management can now be organically linked with the production site. The Solut...
...ight analog inputs can be connected for each Unit. • There is isolation between input channels, so unwanted circuit paths between thermocouple inputs can be prevented. • Output scaling (±32,0...
...ight analog inputs can be connected for each Unit. • There is isolation between input channels, so unwanted circuit paths between thermocouple inputs can be prevented. (Except for CS1W-PTR01/...
...e active CPU Unit, the standby CPU Unit takes over in an instant (using the hot standby method) so that system operation continues essentially unaffected. Other duplex variations are also pos...
...L, INT, BCD, or STRING. Data configuration files required for the host computer can be created, so necessary data can be retrieved even if the SPU is mounted in a device after the PLC is alre...
...nnovative new lock structure makes connection extremely simple. The lock mechanism is internal, so it will no longer become jammed by sputtered fluids or dust. Also, the use of a movable lock...
...ous models from OMRON. The protective structure eliminates the need for screws to hold a cover, so there are no worries about loose screws leading to liquid penetration. And the model number ...
...s with very few failures. Massive System Variation We provide a wide variety of RFID components so that users can customize configurations for any installation space or objective, from replac...
...system, with its highly stable light source, can be turned off when illumination is not needed. So, electricity costs can be reduced. (For a lamp system whose light source is unstable, you ha...
...unications baud rate is set without using switches and addresses are set using rotary switches, so setting errors are reduced. • Communications connector and removable I/O terminal block enab...
...DC and Low Voltage 24 to 48 VAC/12 to 48 VDC. • ON- and OFF-times can be set independently and so combinations of long ON- or OFF-time and short OFF- or ONtime settings are possible. • Twen...
... design. It offers greater performance and faster I/O response as well as extreme scalability - so you will only need one family. In addition, programming, debugging and networking are faster...
... to maintain a stable measurement. They are also susceptible to the influences of ambient light so are difficult to measure using conventional laser measurement sensors. The ZG2 solves these ...